2020-11-06 11:39 PM
Hello.
I am looking for example of External Qspi Loader for the Stm32h743.
I manage to make my functions work. but not to create the .stldr
I have the impression that he does not take Init.
I am under Stm32cubeide.
thank you
2020-11-09 2:53 AM
Hi @cVass.1
You can refer to available QSPI examples with STM32CubeH7 firmware: STM32Cube_FW_H7_V1.6.0\Projects\STM32H743I-EVAL\Examples\QSPI
Bouraoui
2020-11-09 11:42 PM
thank you,
but no example to create an External Loader.
On my tests I must do a Disconnect and Connect to manage to put in Mapping.
2020-11-11 5:19 AM
Hi @cVass.1
You can refer to application note "Quad-SPI interface on STM32 microcontrollers and microprocessors" AN4760
Bouraoui
2020-11-13 1:07 PM
hello, whatever progress a Read gives me an error message.
Here I do a Disconnect then a Connect, it works
Do you have an idea
thank you
2020-11-26 2:21 AM
Hi cVass.1
I'm struggling with the same problem. I've created required functions, tested them in the stm32cubeide and everything looks OK. I managed read and write an external flash (1M). Then I added Loader_Src.c and Dev_Inf to the project and built it with the linker (please find attachment). I got .stldr and copied it to the appropriate folder of the STM32CubeProgrammer. Now I can read the external flash by STM32CubeProgrammer, but unfortunatelly cannot erase and write. The error message says: failed to erase memory... Please let me know if you have some progress.
Thanks
2020-11-26 4:17 AM
hello can you send me the complete project. Thank you
2020-11-26 10:01 AM
Hello
my Linker is identical
can you show me my Loader_Src and Dev_Inf.
Thank you
2020-12-14 8:55 AM
Hi @cVass.1
Can you share your project and the target memory's datasheet?
Bouraoui
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.