2014-03-02 10:38 AM
Hi. I'm currently in a group who are building an ROV and using the stm32f100rb to controll 7 rc motors. The issue I'm having is when outputting a pwm signal to a osciloscop I get a very rough resolution. The signal is supposed to be between 1 ms and 2 ms, and I would like to atleast be able to set the width to 1,00 to 2,00 ms (100 steps). When I alter the width now, i only get 1,0ms 1,2ms, 1,4ms, 1,6ms, 1,8ms and 2,0 ms. It rounds of to the closest one. Anybody knows what might be the problem?
#stm32 #pwm #discovery #output2014-03-02 3:54 PM
As I have to guess what you've coded I might presume your prescaler is too large.
I've posted servo code in the past[DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32VLDiscovery/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32VLDiscovery/Servo%20control%20using%20STM32VLDiscovery&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000491D59B8574F8049B5DFA3E8B21CBA51¤tviews=2039]https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32VLDiscovery/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2FSTM32VLDiscovery%2FServo%20control%20using%20STM32VLDiscovery&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000491D59B8574F8049B5DFA3E8B21CBA51¤tviews=20392014-03-03 1:58 AM
Thanx for the fast answer. Sorry, forgot to post the code. Here's what I've got:
int main(void){ initialization_Timers(); PWM_Truster_1_width(1000); while(1){ }}void initialization_Timers (void){ RCC_Configuration(); //(Must be before GPIO_timer_config!) GPIO_timer_config(); TIM_periode= 20000-1; PrescalerValue =24-1; /* Time base configuration */ TIM_TimeBaseStructure.TIM_Period = TIM_periode; TIM_TimeBaseStructure.TIM_Prescaler = PrescalerValue; TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; //initialization of timer 2 TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure); //initialization of timer 3 TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure); /* TIM2 enable counter */ TIM_Cmd(TIM2, ENABLE); /* TIM3 enable counter */ TIM_Cmd(TIM3, ENABLE); /*set's the initial values for the PWM-outputs PWM_Truster_1_width(1500); }void PWM_Truster_1_width(uint16_t width){ width_1=width; TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse =width;//width;//endre her TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High; TIM_OC1Init(TIM2, &TIM_OCInitStructure); TIM_OC1PreloadConfig(TIM2, TIM_OCPreload_Enable);}Can you spot whats wrong?2014-03-03 6:38 AM
If you are running the the buses at 24 MHz, the period should be 20 ms (50 Hz) confirm that.
The width should be programmable with 1 us granularity, as the timer is clocking at 1 MHz.2014-03-03 8:45 AM
Yes, the periode time is 20 ms, and I also get a pulse between 1 and 2 ms, but its a realy course resolution as I'm only able to change it by 0,2 ms either way.
2014-03-03 10:44 AM
You should be able to change the pulse width in 1 micro-second units, if you can only resolved 0.2 ms (200 us) then I'd have to question how you are measuring the signal.
2014-03-04 1:03 AM
Thanx for all your help. Just found out the scope was calibrated wrong. So, sorry for bothering you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.