STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F103RBT6 basic requirement to load program with SWD

Posted on January 28, 2014 at 10:50Hi! I have been playing with a STM32f103rbt6 chinese board for the last few months, it's working well. I am using the SWD of my stm32F4 discovery to upload the program. Now i wanted to make my own board, so i desig...

jean2 by Associate II
  • 8132 Views
  • 19 replies
  • 0 kudos

STM32F051 with SPI: no reception

Posted on March 04, 2014 at 12:10Hi,I have the SPI communication working but do not receive the answer of the slave. I can see the answer on the scope but not in the controller. Can anybody help ?My main.c/* Includes --------------------------------...

0690X000006056DQAQ.png

PWM Signals

Posted on March 02, 2014 at 19:38Hi. I'm currently in a group who are building an ROV and using the stm32f100rb to controll 7 rc motors. The issue I'm having is when outputting a pwm signal to a osciloscop I get a very rough resolution. The signal i...

smvhauge by Associate II
  • 2323 Views
  • 6 replies
  • 0 kudos

spi speed configuration of STM32L

Posted on March 04, 2014 at 00:42Hi all,I am playing with SPI examples of STM32L recently and would like to ask a simple question about the SPI clock rate.  When I read through the datasheet, it mentions APB1 and APB2 have maximal frequency of 32MHz...

STM32F4 UART programming

Posted on July 30, 2013 at 10:08I have managed to make Flash loader demonstrator work with my FTDI. Whenever I want to connect to my STM32F4 Discovery board I have to do that in two steps. Firstly I connect proper pins from FTDI to PCB, then I open ...

jernej by Associate
  • 4238 Views
  • 8 replies
  • 0 kudos

software i2c not working..

Posted on March 09, 2012 at 16:41Want to read my LIS302 sensor with software I2C (bit banging)Hardware i2c works.Here is some code.Please help me with software i2c...http://pastebin.com/d0M9jRaY

hitsumen by Associate II
  • 6327 Views
  • 21 replies
  • 0 kudos

Lan8720 interrupt pin

Posted on March 03, 2014 at 16:35Hello everybody. I want to use lan8720 ethernet interface with the interrupt pin. But the interrupt pin is the same with the refclk out. So if I use anexternal 25Mhz clock, or the stm32f4 mco pin, need to connect the...

totti001 by Associate II
  • 1494 Views
  • 2 replies
  • 0 kudos

How to use DSP library with STM32L1xx on IAR?

Posted on March 02, 2014 at 16:14Hello,I want to use DSP library functions on STM32L1xx.STM32L1xx is using ARM-cortex M3, same as STM32F1xx. How can I include the DSP library (ST library or CMSIS library) to a project?Thanks #stm32l1xx-and-dsp-li...

zoharr by Associate II
  • 1753 Views
  • 2 replies
  • 0 kudos

ADC is triggered by timer

Posted on March 03, 2014 at 11:28 Helllooooooooo,I want to use the configured timer as a trigger for the A/D converter. I have to set up an interrupt service routine (that will be called when new data is ready to be read) to read the data and fill a...

shiva by Associate
  • 1033 Views
  • 1 replies
  • 0 kudos

Preload register

Posted on March 03, 2014 at 10:37Hello,I'm new in microcontroller world and have a question. What is preload register in TIM3? I really don't understand it's meaning. So could somebody help me, please. #preload-register

karolina by Associate II
  • 1705 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.