2016-03-07 4:47 PM
I am using the STM32L053 MCU on the Nucleo board. The MCU is powered by 1.8V during the test. If I add some delay after turnning on the PVD, then the PVDO bit returns 1, with no delay it returns 0.
I could not find how long it takes for the PVDO bit to become valid in the datasheet. Has anyone tested that? Here is the initialise routine:void
PVD_Config(
void
)
{
/*##-1- Enable Power Clock #################################################*/
__PWR_CLK_ENABLE();
/* Wait for internal VREF ready */
while
( 0 == __HAL_PWR_GET_FLAG( PWR_FLAG_VREFINTRDY ) );
/*##-2- Configure the NVIC for PVD #########################################*/
HAL_NVIC_SetPriority(PVD_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(PVD_IRQn);
sConfigPVD.PVDLevel = PVD_THRESHOLD_1V9;
sConfigPVD.Mode = PWR_MODE_IT_RISING_FALLING;
HAL_PWR_PVDConfig(&sConfigPVD);
/* Enable the PVD */
HAL_PWR_EnablePVD();
/* Add some delay here */
if
( 0 == __HAL_PWR_GET_FLAG( PWR_FLAG_PVDO ) )
{
/* Do something */
}
}
2016-03-10 2:18 AM
Hi liu.bill.003,
I think the behaviour that you see is related to your voltage supply satatus. The PVD is working, and the PVDO flag is switching between 1 and 0 to indicate a change in VDD level comparing to the programmable voltage threshold.
As mentioned about PVDO, in STM32L0 reference manual below
:
Bit 2
PVDO:
PVD output
This bit is set and cleared by hardware. It is valid only if PVD is enabled by the PVDE bit.
0: V
DD
is higher than the PVD threshold selected with the PLS[2:0] bits.
1: V
DD
is lower than the PVD threshold selected with the PLS[2:0] bits.
Note: The PVD is stopped by Standby mode. For this reason, this bit is equal to 0 after
Standby or reset until the PVDE b
i
t is set.-Hannibal-
2016-03-14 4:53 PM
Hi Hannibal,
Thanks for your reply. Today I solved my problem. The flag I am polling for Vrefint_ready is wrong. The correct bit is SYSCFG_CFGR3_VREFINT_RDYF. No delay is required after enabling PVD. The corrected polling code is pasted below./* Wait for internal VREF ready */
__SYSCFG_CLK_ENABLE();
while
( 0 == __HAL_SYSCFG_GET_FLAG( SYSCFG_FLAG_VREF_READY ) );
2016-03-15 2:58 AM
Hi liu.bill.003,
It's good that you have find the right way to your need. Thanks for your contribution.-Hannibal-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.