2025-01-16 8:20 PM - last edited on 2025-03-24 1:49 AM by Amel NASRI
Originally posted as a comment on the How to write your question to maximize your chances to find a solution article.
Moved to the forum for clarification & better discussion.
How to create programming code based on the information ?
2025-01-16 8:38 PM - last edited on 2025-01-20 1:16 AM by Andrew Neil
Merged from separate thread.
I would like to ask if this device can read input digital and analog signals 5 volts and output 5 volts on and off in milliseconds STM32F412G-DISCO. Who can help create programming code based on information ?
Discovery Development Board, STM32F412ZG, 32bit, ARM Cortex-M4 or any other boards ? Described diagram is available that shows and describes the relation between pulse number and IO pin On/Off
Thanks in advance for your answer !
2025-01-16 8:39 PM
> Who can help create programming code based on information ?
2025-01-17 2:08 AM
Please clarify what you're actually asking for?
The article describes the information you need to give in your post when asking a question.
2025-01-24 8:42 PM
3) Output pin 9 is LED1
4) Output pin 10 is LED2
At start up the engine both LEDs go HIGH every half cycle at pulse 30 till 33 until the system completes 604 cycles = 70064 pulses then reset to zero.
Reference sensor toggle LED1 at pulse 20 to set LED1 high in every half cycle and then LED2 high at pulse 75-78 and so on loop.
LED2 ON at pulse 75
LED2 ON at pulse 76
LED2 ON at pulse 77
LED2 ON at pulse 78
Cycle reset. Starting a new cycle
LED1 ON at pulse 17
LED1 ON at pulse 18
LED1 ON at pulse 19
LED1 ON at pulse 20
Then looping continue.
Reluctor wheel has 60-2 teeth = 58 pulses and two missing pulses is the gap. One pulse takes 1.38ms at the engine speed RPM750.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.