2025-01-24 10:44 AM
Hi,
I have been making a lot of calls into null pointers and am quite surprised at the results. I am expecting hard failures when I make this mistake but instead it seems that things just keep going and it takes a long time to realize I failed to initialize a pointer.
e.g.
LL_UCPD_RxEnable(Ports[PortNum].husbpd);I have made this call which resolves to
#define SET_BIT(REG, BIT) ((REG) |= (BIT))
__STATIC_INLINE void LL_UCPD_RxEnable(UCPD_TypeDef *UCPDx)
{
SET_BIT(UCPDx->CR, UCPD_CR_PHYRXEN);
}I have made this with the value husbpd uninitialized. But nothing negative happens other than the operation doesn't complete. No crash or other error.
Is there anything I can do or enable that will produce a harder fault when I make this mistake?
2025-01-24 12:42 PM
There is memory mapped at ZERO, usually determined by the BOOTx pins
Perhaps enable asserts() so the library sanity checks the pointers/parameters passed into the HAL upper layers.
It will not help here, as it's not being checked.
You could fill uninitialized memory with 0xCDCDCDCD type pattern, or something similar, that's more likely to throw a fault when used.
Other Cortex-Mx parts you could perhaps play with watch points, or configure MPU to throw a MemManage_Handler
2025-01-24 6:06 PM
Thanks, ill look deeper. The pointers are all 0. So i guess its doing something there. Maybe I can put something at 0 to like the codes you suggested.
2025-01-24 10:00 PM - edited 2025-01-24 10:06 PM
You could use the Cortex-M memory protection unit:
c - NULL pointer protection with ARM Cortex-M MPU - Stack Overflow
After doing so, read/write access to the protected region(s) will raise the HardFault_Handler:
/* Configure the MPU to prevent NULL-pointer dereferencing ... */
MPU->RBAR = 0x0U /* base address (NULL) */
| MPU_RBAR_VALID_Msk /* valid region */
| (MPU_RBAR_REGION_Msk & 7U); /* region #7 */
MPU->RASR = (7U << MPU_RASR_SIZE_Pos) /* 2^(7+1) region, see NOTE0 */
| (0x0U << MPU_RASR_AP_Pos) /* no-access region */
| MPU_RASR_ENABLE_Msk; /* region enable */
MPU->CTRL = MPU_CTRL_PRIVDEFENA_Msk /* enable background region */
| MPU_CTRL_ENABLE_Msk; /* enable the MPU */
__ISB();
__DSB();
// ...
*(int*)NULL = 0x1234; // triggers hard fault handler
hth
KnarfB
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.