2019-05-09 6:36 AM
So somehow through my chain of execution I end up here
void _exit (int status)
{
_kill(status, -1);
while (1) {} /* Make sure we hang here */
}
From disassembly it seems that the functions preceeding it are
ITM_SendChar()
and before that
HAL_CAN_RxFifo1MsgPendingCallback()
I do use HAL_CAN_RxFifo1MsgPendingCallback(), but following in from there I do not know how it ends up in ITM_SendChar nor how does this lead to the _exit() function.
I've had errros before with HardFaultHandler(), but never ended up in _exit() and not sure how to proceed.
I am using TrueStudio, I started using it over Keil as it seemed to be better at dynamic printf and array display. It does show some issues as at 2,000,000 bps it drops bytes in between DMA transfers while the same code in Keil wouldn't.
Toolchain: Atollic ARM Tools
Probe: ST_Link
Optimisation: None (-O0)
Debugging: Maximum (-g3)
MCU: STM32F407
2019-05-09 6:40 AM
What tool-chain?
Malloc? _sbrk?
Disassemble the complete object code, and cross-reference where _exit is being called. As I recall FromELF and/or objcopy contain dissemblers.
Break-point _exit() look at the value of LR, or stacked version thereof, to work back up the call-stack.
2019-05-09 8:53 AM
I use malloc for circular buffers, they are used constantly and are not freed.
Not sure about _sbrk, I didn't touch it in any way.
"Disassemble the complete object code, and cross-reference where _exit is being called" how to do thate exactly?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.