2013-07-26 3:06 AM
Hi, i've got a problem with leaving from standby mode, both by RTC Alarm and WKUP pin. This is my code:
int main( void ) { #ifdef DEBUG debug(); #endif prvSetupHardware(); GPIOC->ODR |= (u16)0x0040; PWR_EnterSTANDBYMode(); GPIOC->ODR &= (u16)~0x0040; while (1) {}; } static void prvSetupHardware( void ) { RCC_APB2PeriphClockCmd( RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOB |RCC_APB2Periph_GPIOC | RCC_APB2Periph_GPIOD | RCC_APB2Periph_GPIOE | RCC_APB2Periph_AFIO, ENABLE ); NVIC_SetVectorTable( NVIC_VectTab_FLASH, 0x0 ); NVIC_PriorityGroupConfig( NVIC_PriorityGroup_4 ); vLedInitialise(); vEXTI_Configuration(); vNVIC_Configuration(); vRTC_Configuration(); PWR_WakeUpPinCmd(ENABLE); } void vEXTI_Configuration( void ) { EXTI_InitTypeDef EXTI_InitStructure; /* Configure EXTI Line17(RTC Alarm) to generate an interrupt on rising edge */ EXTI_ClearITPendingBit(EXTI_Line17); EXTI_InitStructure.EXTI_Line = EXTI_Line17; EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt; EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Rising; EXTI_InitStructure.EXTI_LineCmd = ENABLE; EXTI_Init(&EXTI_InitStructure); } /*-----------------------------------------------------------*/ void vNVIC_Configuration( void ) { NVIC_InitTypeDef NVIC_InitStructure; /* Configure one bit for preemption priority */ NVIC_PriorityGroupConfig(NVIC_PriorityGroup_1); /*Enable the RTC Alarm Interrupt*/ NVIC_InitStructure.NVIC_IRQChannel = RTCAlarm_IRQChannel; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); } /*-----------------------------------------------------------*/ void vRTC_Configuration( void ) { RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR | RCC_APB1Periph_BKP, ENABLE); /* Allow access to BKP Domain */ PWR->CR |= 0x00000100; RCC_LSEConfig(RCC_LSE_ON); while (RCC_GetFlagStatus(RCC_FLAG_LSERDY) == RESET) {} RCC_RTCCLKConfig(RCC_RTCCLKSource_LSE); RCC_RTCCLKCmd(ENABLE); RTC_WaitForSynchro(); RTC_WaitForLastTask(); RTC_ITConfig(RTC_IT_ALR, ENABLE); RTC_WaitForLastTask(); RTC_SetPrescaler(32767); RTC_WaitForLastTask(); while ( RTC_GetFlagStatus( RTC_FLAG_SEC ) == RESET ) {} RTC_SetAlarm(5); RTC_WaitForLastTask(); } void RTCAlarm_IRQHandler( void ) { GPIOC->ODR ^= 0x00000080; EXTI_ClearITPendingBit(EXTI_Line17); if (PWR_GetFlagStatus(PWR_FLAG_WU) != RESET) PWR_ClearFlag(PWR_FLAG_WU); RTC_WaitForLastTask(); RTC_ClearITPendingBit(RTC_IT_ALR); RTC_WaitForLastTask(); } I know that EXTI isn't necessary to wake MCU up from standby mode, but I tried the same code with Stop Mode and it works. Another issue is strange operation with debugger (JLINK) connected to the eval board - with Stop mode I had to abort debug session, and reset MCU. In standby mode I tried with connected or disconnected debugger and it has never worked. Could anyone help me? Regards #stm32-standby-wake-rtc #wkup2013-07-26 4:29 AM
What part is this with?
Do you enable the GPIO pins somewhere? Generally you're not going to be able to use hardware debugging to function across events that power down the core. You need to change your testing to output diagnostic/telemetry information via a serial port. When you reset you don't want to mess with the full RTC setup if this is a STANDBY RESET, look at some of the PWR\STANDBY project examples2013-07-26 4:41 AM
Thanks for reply. I use STMF103. Problem with WKUP pin is solved - simply on my eval board this pin is connected to Vcc via a series resistor. When I shorted it to ground then forced MCU to get into standby mode and connect pin to Vcc - MCU waked up. But with RTC it still doesn't work (I tested it with WKUP pin shorted to ground).
Yes, I know that after reset I don't need to reconfigure RTC from scratchWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.