2017-10-28 3:45 AM
I have my own product board with STM32L073VBT6.The power comsumption increase to 10mA (an other is 4mA) when enter low power mode.So I had removed all other chips only left the STM32 and found out that the MCU cost the 10mA. The function of the chip is ok. I Don't understand How the chip came to that with the function ok.
?????STM32L073??pCB????????10mA??????????????IC??????????3?mA????????????????????????
#stm32l073 #low-power-run #issue2017-10-28 7:47 AM
Unfortunately your post lacks sufficient detail to replicate or understand the circuit and software as implemented.
Is this with a debugger attached?
How to you make a determination about the internal state of the processor?
Sleep/Standby?
External buffers, LEDs, pull up/down resistors?
2017-11-07 5:27 PM
Just power on with 3.3 the mcu,and connect the reset pin to gnd.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.