2015-11-06 3:55 AM
Hello.
My colleague is in trouble about NVIC of STM32L053.. At the moment, he wants to use several external interrupts; some of them are assigned to EXTI line 0, some others are assigned to EXTI line 1, and the rest are assigned to EXTI line2. According to him, EXTI line 0 doesn't work at all regardless edge trigger happens. Also some interrupts of line 1 and line 2 don't work at all regardless edge triggger happnes as well. Does he take care of setting register when he assigns several interrupt to the same vector ? If someone can offer a sample program to solve this issue, I appreciate it. Regards #n2015-11-06 5:13 AM
Perhaps if you show some code it might be more apparent why it isn't working.
What board is being used, and are the pins free/available?Is the SYSCFG peripheral enabled? What settings are written to the NVIC and EXTI? Can you read these registers back to confirm the settings, and those for the associated GPIO?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.