2019-09-25 4:56 PM
Hello everyone, i would like to connect STM32F7 with multiple SDRAMs because i would like to get at least 256 MByte, i spent too much time trying to search for a detailed way, how to connect at first more thant one SDRAM together and then to connect them with STM32F7. but i couldn't find out. can someone please provide me with these informations.
Thanks.
2019-09-25 5:06 PM
It supports TWO banks, one at 0xC0000000 the other at 0xD0000000
As I recall the interface to both is the same, but there are two chip select signals SDNE[1:0] and two clock enables SDCKE[1:0]
I'm sure this is covered in one of the Reference Manuals
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.