2012-02-29 4:22 AM
Hi,
I'm almost done finishing my STM32F4 Eval Board. But I still have a few questions: I want to use the internal regulator so I connected Vcap1 and Vcap2 with cap's. There is still this PDR_ON Pin. should i leave it unconnected? I don't really need the internal reset afterpPower-down function. with regards Alex2012-02-29 7:55 AM
OK ST updated the datasheet.
@LQFP100 connect to VSS (cause its now always internal ON) @LQFPB144/176 take look at the figure2012-03-06 4:00 AM
But in the STM32F40x and STM32F41x datasheets in the pin diagram of LQFP100 in figure 11, chapter 3, the pin 99 still has the name ''PDR_ON''. This is misleading. It would be better, if the pin 99 is named ''VSS'' there. (at least as I understand it, this Pin 99 now just is VSS pin).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.