2019-03-11 8:26 AM
I want to read the Option Bytes values from my STM32F446 in order to debug strange behavior. On what addresses do they reside? According to the Reference Manual they reside on addresses 0x1FFFC000 and 0x1FFFC008, but when I look at the implementation of HAL_FLASHEx_OBGetConfig it is reading from addresses OPTCR_BYTE0_ADDRESS, OPTCR_BYTE1_ADDRESS, OPTCR_BYTE2_ADDRESS, and OPTCR_BYTE3_ADDRESS (0x40023C14 - 0x40023C17). Can someone please clarify?
2019-11-25 7:39 AM
IMO all bits described in Table 9 - which are also "mirrored" in FLASH_OPTCR - are subject to programming according to section 3.6.2. In other words, you program then all at once.
Terminology is always confusing - this is a live topic, with a huge amount of concepts and details, which are sometimes hard to describe precisely without resorting to excessive explanation; and with many changes as the chips are evolving and are updated and their features expanded. Users are often expected to have prior knowledge to fill out the gaps. This is not to say documentation can't or shouldn't be improved; it's just that it's a hard task. Maybe you might want to suggest particular improvements yourself.
You may not be aware of the fact that this is a primarily user driven forum, with casual ST presence. I am not ST. If you want to pick up the issue of imprecise terminology used in the manuals, maybe you want to contact ST directly, through the web support form, or through your FAE.
JW
@Imen DAHMEN , could perhaps 3.6.2 in RM0390 - and all other analogous chapters in other STM32 RMs - be made less ambiguous by omitting the "user" from "user option bytes", as 3.6.2. appears to refer to programming of all option bytes, whereas "user option bytes" appear to designate only a portion of the overall option bytes?
2019-11-25 7:47 AM
@Vincent Onde ,
Can't this issue be clarified within an AN, together with an overview of the various features which can be enabled/disabled using the Option bits/bytes accross all the STM32 families?
JW
2019-11-25 8:04 AM
I'm on vacation right now, but when I get back I will try to change all bits and see if I can successfully update them using the instructions in 3.6.2 (and hence, not use the HAL-functions). Thank you for your help.
2019-12-02 5:58 AM
Accidental double-post.
2019-12-02 6:56 AM
I tried the following code:
#define OPTION_BYTES_MASK (0b10000000111111111111111111101100)
#define OPTION_BYTES_FROM_FLASH ((((uint32_t) *((volatile uint16_t*)0x1FFFC008)) << 16) | \
(((uint32_t) *((volatile uint16_t*)0x1FFFC000)) << 0))
#define DESIRED_OPTION_BYTES ((((uint32_t) OB_PCROP_DESELECTED) << 24) | \
(((uint32_t) 0xFF) << 16) | \
(((uint32_t) OB_RDP_LEVEL_0) << 8) | \
(((uint32_t) (OB_STDBY_NO_RST | OB_STOP_NO_RST | OB_IWDG_SW | OB_BOR_LEVEL3)) << 0))
void updateOptionBytesIfNecessary() {
if ((DESIRED_OPTION_BYTES != (OPTION_BYTES_FROM_FLASH & OPTION_BYTES_MASK)) ||
(DESIRED_OPTION_BYTES != (FLASH->OPTCR & OPTION_BYTES_MASK))) {
FLASH->OPTKEYR = FLASH_OPT_KEY1; // Unlock option bytes
FLASH->OPTKEYR = FLASH_OPT_KEY2; // Unlock option bytes
while(FLASH->SR & FLASH_SR_BSY) { } // Wait until busy flag goes low
FLASH->OPTCR = DESIRED_OPTION_BYTES; // Update the Option Bytes
FLASH->OPTCR |= FLASH_OPTCR_OPTSTRT; // Set the option start bit
while(FLASH->SR & FLASH_SR_BSY) { } // Wait until busy flag goes low
FLASH->OPTCR |= FLASH_OPTCR_OPTLOCK; // Lock the flash
}
}The code above can successfully update nRST_STDBY, rRST_STOP, WDG_SW, BOR-level, Read Protection Level 1 -> Read Protection Level 0, and nWRT as long as SPRMOD is 0. If SPRMOD is 1, then it will not update SPRMOD or nWRT. Does anybody know what's wrong?
2019-12-02 7:34 AM
I guess I have found the reason why SPRMOD can't be changed from 1 to 0. From the reference manual, section "Proprietary code readout protection (PCROP)":
"The deactivation of the SPRMOD and/or the unprotection of PCROPed user sectors can only occur when, at the same time, the RDP level changes from 1 to 0. If this condition is not respected, the user option byte modification is canceled and the write error WRPERR flag is set. The modification of the users option bytes (BOR_LEV, RST_STDBY, ..) is allowed since none of the active nWRPi bits is reset and SPRMOD is kept active."
Does this mean setting SPRMOD 1 -> 0 needs to be done in 3 steps, first setting Read Protection (RDP) to level 1, then setting SPRMOD to 0, and then setting Read Protection (RDP) back to level 0?
2019-12-02 2:44 PM
AFAIK this is what STLink Utility does too. This implicitly involves bulkerase, so it is rather time consuming.
I'm not sure why do you want to do this, but at this point it sounds that you already know more than me on this issue, so I can't help you anymore... :)
JW
2019-12-03 2:33 AM
I think I solved it!!! A little disappointing that the HAL-function doesn't take the SPRMOD == 1 special case into account.
#define LOG_STRING(__STRING__,__POST_TRANSMISSION_OPTION__)
#define OPTION_BYTES_MASK (0b10000000111111111111111111101100)
#define OPTION_BYTES_FROM_FLASH ((((uint32_t) *((volatile uint16_t*)0x1FFFC008)) << 16) | \
(((uint32_t) *((volatile uint16_t*)0x1FFFC000)) << 0))
#define DESIRED_OPTION_BYTES ((((uint32_t) OB_PCROP_DESELECTED) << 24) | \
(((uint32_t) 0xFF) << 16) | \
(((uint32_t) OB_RDP_LEVEL_0) << 8) | \
(((uint32_t) (OB_STDBY_NO_RST | OB_STOP_NO_RST | OB_IWDG_SW | OB_BOR_LEVEL3)) << 0))
void updateOptionBytesIfNecessary() {
if (DESIRED_OPTION_BYTES == (OPTION_BYTES_FROM_FLASH & OPTION_BYTES_MASK)) {
LOG_STRING("\r\nOption bytes are already up-to-date", SWITCH_TO_Rx_MODE_WHEN_DONE);
return;
}
LOG_STRING("\r\nOption bytes need updating", STAY_IN_Tx_MODE_WHEN_DONE);
uint8_t SPRMOD = (uint8_t)(OPTION_BYTES_FROM_FLASH >> 31);
uint8_t RDP_LEVEL = (((uint8_t)(OPTION_BYTES_FROM_FLASH >> 8)) == OB_RDP_LEVEL_0) ? OB_RDP_LEVEL_0 :
((((uint8_t)(OPTION_BYTES_FROM_FLASH >> 8)) == OB_RDP_LEVEL_2) ? OB_RDP_LEVEL_2 : OB_RDP_LEVEL_1);
Bool_t flashWillBeErased = (Bool_t)((SPRMOD == 1) || (RDP_LEVEL != OB_RDP_LEVEL_0));
FLASH->OPTKEYR = FLASH_OPT_KEY1; // Unlock option bytes
FLASH->OPTKEYR = FLASH_OPT_KEY2; // Unlock option bytes
while(FLASH->SR & FLASH_SR_BSY) { } // Wait until busy flag goes low
if (SPRMOD == 1) {
LOG_STRING("\r\nSPRMOD was 1. Weird special case needed!!!", STAY_IN_Tx_MODE_WHEN_DONE);
// SPRMOD is 1. We need to change the Read Protection (RDP) level to 1 (weird, but that's what the Ref Manual says)
if (RDP_LEVEL != OB_RDP_LEVEL_1) {
LOG_STRING("\r\***_RDP_LEVEL_1 was not used. Will need to set to OB_RDP_LEVEL_1", STAY_IN_Tx_MODE_WHEN_DONE);
// FLASH->OPTCR = ((FLASH->OPTCR & 0xFFFF00FF) | (((uint32_t)(OB_RDP_LEVEL_1)) << 8)) & OPTION_BYTES_MASK; // Doesn't work for mysterious reasons!!!
*(volatile uint8_t*)OPTCR_BYTE1_ADDRESS = OB_RDP_LEVEL_1; // Weird, we must only write to the particular byte in the FLASH->OPTCR register
FLASH->OPTCR |= FLASH_OPTCR_OPTSTRT; // Set the option start bit
while(FLASH->SR & FLASH_SR_BSY) { } // Wait until busy flag goes low
} else {
LOG_STRING("\r\***_RDP_LEVEL_1 was used. No need to update it", STAY_IN_Tx_MODE_WHEN_DONE);
}
} else {
LOG_STRING("\r\nSPRMOD was 0. No special case needed", STAY_IN_Tx_MODE_WHEN_DONE);
}
if (flashWillBeErased) {
LOG_STRING("\r\nEntire flash will now be erased, don't expect any more logging messages like this one", SWITCH_TO_Rx_MODE_WHEN_DONE);
}
FLASH->OPTCR = DESIRED_OPTION_BYTES; // Update the Option Bytes
FLASH->OPTCR |= FLASH_OPTCR_OPTSTRT; // Set the option start bit
while(FLASH->SR & FLASH_SR_BSY) { } // Wait until busy flag goes low
FLASH->OPTCR |= FLASH_OPTCR_OPTLOCK; // Lock the flash
LOG_STRING("\r\nNow finished updating option bytes", SWITCH_TO_Rx_MODE_WHEN_DONE);
}
2019-12-03 3:00 PM
Arnold,
Thanks for sharing this!
// FLASH->OPTCR = ((FLASH->OPTCR & 0xFFFF00FF) | (((uint32_t)(OB_RDP_LEVEL_1)) << 8)) & OPTION_BYTES_MASK; // Doesn't work for mysterious reasons!!!
*(volatile uint8_t*)OPTCR_BYTE1_ADDRESS = OB_RDP_LEVEL_1; // Weird, we must only write to the particular byte in the FLASH->OPTCR registerHummm.
I wonder - your skills are way off of those of the usual Cube/HAL users, why do you use it?
Jan
2019-12-04 1:07 AM
Thank you for the kind words. I usually use Cube/HAL as a starting point (they're quite good when they work), but when I'm finished with my code usually there aren't many similarities with the original code left.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.