2021-08-11 12:42 PM
I would like to be able to write debugging messages to a serial terminal. Is there sample code that does this? Is there something I need to know about setting up clocks that is special for ST-LINK v3? How does one know which uart is connected to ST-LINK? Is it on pin PF9?
2021-08-11 12:59 PM
>>Is it on pin PF9
No
And the PG9/PG14 connections are on the ST-LINK IC, not the H753
That would be EVAL2 (MB1246 RevE) board, there should be jumpers to allow selection between RS232 connector or the ST-LINK, on USART1
JP7 / JP8
PB14 / PB15
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.