2022-07-08 12:02 PM
We also configured the other PAx pins, such as PA0, PA1, PA4, PA5, ect as ADC channels. these pins work properly.
Removing SB13 and SB14 is based on the suggestion of NUCLEO-L073RZ manual (UM1724 Rev 14), in order to use PA2/3 pins.
Please let us know on how to use PA2/3 pins as Analog Inputs.
Thanks
David
2022-07-08 1:52 PM
> AP2 and PA3 don't read any analogy inputs
What does this mean? Does the program crash? How are these pins connected? If you set them as GPIO output and toggle, do you see valid logic levels on them?
JW
2022-07-08 10:52 PM
In CubeMX is this pins green?
2022-07-09 12:32 AM
Did you put the resistors/jumpers in the new places (SB62/63)? This is necessary to connect PA2/3 to the connector's pins.
2022-07-11 4:44 PM
Have you guys even used any of STM32 Nucleo-64 boards and configured PA2/3 as Analog Input?
All of STM32 Nucleo-64 boards have the same pin setting.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.