2025-09-28 11:29 PM - last edited on 2025-09-29 1:38 AM by Imen.D
Hi~
NUCLEO H563ZI USART GPDMA channel6 not received buffer.
static void MX_USART6_UART_Init(void)
/* GPDMA2_REQUEST_USART6_RX Init */
NodeConfig.DestAllocatedPort = LL_DMA_DEST_ALLOCATED_PORT1;
NodeConfig.DestHWordExchange = LL_DMA_DEST_HALFWORD_PRESERVE;
NodeConfig.DestByteExchange = LL_DMA_DEST_BYTE_PRESERVE;
NodeConfig.DestBurstLength = 1;
NodeConfig.DestIncMode = LL_DMA_DEST_INCREMENT;
NodeConfig.DestDataWidth = LL_DMA_DEST_DATAWIDTH_BYTE;
NodeConfig.SrcAllocatedPort = LL_DMA_SRC_ALLOCATED_PORT0;
NodeConfig.SrcByteExchange = LL_DMA_SRC_BYTE_PRESERVE;
NodeConfig.DataAlignment = LL_DMA_DATA_ALIGN_ZEROPADD;
NodeConfig.SrcBurstLength = 1;
NodeConfig.SrcIncMode = LL_DMA_SRC_FIXED;
NodeConfig.SrcDataWidth = LL_DMA_SRC_DATAWIDTH_BYTE;
NodeConfig.TransferEventMode = LL_DMA_TCEM_LAST_LLITEM_TRANSFER;
NodeConfig.Mode = LL_DMA_NORMAL;
NodeConfig.TriggerPolarity = LL_DMA_TRIG_POLARITY_MASKED;
NodeConfig.BlkHWRequest = LL_DMA_HWREQUEST_SINGLEBURST;
NodeConfig.Direction = LL_DMA_DIRECTION_PERIPH_TO_MEMORY;
NodeConfig.Request = LL_GPDMA2_REQUEST_USART6_RX;
NodeConfig.BlkRptCount = 1;
NodeConfig.UpdateRegisters = (LL_DMA_UPDATE_CTR1 | LL_DMA_UPDATE_CTR2 | LL_DMA_UPDATE_CBR1 | LL_DMA_UPDATE_CSAR | LL_DMA_UPDATE_CDAR | LL_DMA_UPDATE_CTR3 | LL_DMA_UPDATE_CBR2 | LL_DMA_UPDATE_CLLR);
NodeConfig.NodeType = LL_DMA_GPDMA_LINEAR_NODE;
NodeConfig.SrcAddress = LL_USART_DMA_GetRegAddr(USART6, LL_USART_DMA_REG_DATA_RECEIVE);
NodeConfig.DestAddress = (uint32_t)usart_rx_dma_buffer;
/* Size is always in bytes! Width is determined by source and destination numbers */
NodeConfig.BlkDataLength = sizeof(usart_rx_dma_buffer);
LL_DMA_CreateLinkNode(&NodeConfig, &Node_GPDMA2_Channel6);
LL_DMA_ConnectLinkNode(&Node_GPDMA2_Channel6, LL_DMA_CLLR_OFFSET5, &Node_GPDMA2_Channel6, LL_DMA_CLLR_OFFSET5);
/* Next function call is commented because it will not compile as is. The Node structure address has to be cast to an unsigned int (uint32_t)pNode_DMAxCHy */
/*
*/
LL_DMA_SetLinkedListBaseAddr(GPDMA2, LL_DMA_CHANNEL_6, (uint32_t)&Node_GPDMA2_Channel6);
LL_DMA_ConfigLinkUpdate(GPDMA2, LL_DMA_CHANNEL_6,
(LL_DMA_UPDATE_CTR1 | LL_DMA_UPDATE_CTR2 | LL_DMA_UPDATE_CBR1 | LL_DMA_UPDATE_CSAR
| LL_DMA_UPDATE_CDAR | LL_DMA_UPDATE_CTR3 | LL_DMA_UPDATE_CBR2 | LL_DMA_UPDATE_CLLR),
(uint32_t)&Node_GPDMA2_Channel6);
DMA_InitLinkedListStruct.Priority = LL_DMA_LOW_PRIORITY_LOW_WEIGHT;
DMA_InitLinkedListStruct.LinkStepMode = LL_DMA_LSM_FULL_EXECUTION;
DMA_InitLinkedListStruct.LinkAllocatedPort = LL_DMA_LINK_ALLOCATED_PORT0;
DMA_InitLinkedListStruct.TransferEventMode = LL_DMA_TCEM_LAST_LLITEM_TRANSFER;
LL_DMA_List_Init(GPDMA2, LL_DMA_CHANNEL_6, &DMA_InitLinkedListStruct);
LL_DMA_EnableIT_HT(GPDMA2, LL_DMA_CHANNEL_6);
LL_DMA_EnableIT_TC(GPDMA2, LL_DMA_CHANNEL_6);
/* USART6 interrupt Init */
NVIC_SetPriority(USART6_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),5, 0));
NVIC_EnableIRQ(USART6_IRQn);
/* USER CODE BEGIN USART6_Init 1 */
/* Configure the DMA functional parameters for transmission */
/* USER CODE END USART6_Init 1 */
USART_InitStruct.PrescalerValue = LL_USART_PRESCALER_DIV1;
USART_InitStruct.BaudRate = 115200;
USART_InitStruct.DataWidth = LL_USART_DATAWIDTH_8B;
USART_InitStruct.StopBits = LL_USART_STOPBITS_1;
USART_InitStruct.Parity = LL_USART_PARITY_NONE;
USART_InitStruct.TransferDirection = LL_USART_DIRECTION_TX_RX;
USART_InitStruct.HardwareFlowControl = LL_USART_HWCONTROL_NONE;
USART_InitStruct.OverSampling = LL_USART_OVERSAMPLING_16;
LL_USART_Init(USART6, &USART_InitStruct);
LL_USART_SetTXFIFOThreshold(USART6, LL_USART_FIFOTHRESHOLD_1_8);
LL_USART_SetRXFIFOThreshold(USART6, LL_USART_FIFOTHRESHOLD_1_8);
LL_USART_DisableFIFO(USART6);
LL_USART_ConfigAsyncMode(USART6);
LL_USART_EnableDMAReq_RX(USART6);
LL_USART_EnableIT_IDLE(USART6);
LL_USART_Enable(USART6);
/* USER CODE BEGIN USART6_Init 2 */
LL_DMA_EnableChannel(GPDMA2, LL_DMA_CHANNEL_6);
/* USER CODE END USART6_Init 2 */
========================================================================================
usart_rx_dma_buffer
Only one comes into the buffer and the rest is not filled
please check config.
Edit by ST Moderator to apply source code formatting.
Please see the Posting Tips for how to properly post source code.
2025-09-29 4:51 AM - edited 2025-09-29 4:53 AM
Hi all~
Additionally when i test gpdma2 channel 0 it is working well.
Bue gpdma2 channel6 is not received buffer.
I have to use gpdma channel 6 .
Can you check please~
Thanks~
2025-09-29 4:57 AM
Hello,
You did accept the solution in this thread regarding the same subject but for LPUART, while this one is about USART. Could you please confirm you have solved the issue with LPUART/DMA transfer? did you intentionally accept the solution?
2025-09-29 5:05 AM
Hi
This issue is different lpuart .
Lpuart and usart is woring well in gpdma channel 0.
Please do not confused.
Thanks.
2025-09-29 10:01 AM - edited 2025-09-29 10:06 AM
Hello
Can you check please~
I have not time sorry..
Thanks
2025-10-02 12:57 AM
Hello all
Can Usart use gpdma channel6(2d address) as a cycler?
Please reply~
Thanks.
2025-10-05 5:25 PM
Hello
Please help me
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.