2014-10-14 1:05 AM
Hi,
i bought some Nucleo F103RB Boards and designed a circuit board for the Nucleo to drive my LEDs throught Bluetooth.The prototype with airwires worked perfectly, but know i tried it with my circuit and if i plug the Nucleo on my circuit i got strange behaviour in flash sizes.If i try to flash an image it cannot verify.st-link showed my everytime i run it a different flash size, the sram and page size kept.Here is a sample output:2014-10-14T10:04:07 INFO src/stlink-common.c: Device connected is: F1 Medium-density device, id 0x200364102014-10-14T10:04:07 INFO src/stlink-common.c: SRAM size: 0x5000 bytes (20 KiB), Flash: 0x20000 bytes (128 KiB) in pages of 1024 bytes2014-10-14T10:04:07 INFO gdbserver/gdb-server.c: Chip ID is 00000410, Core ID is 1ba01477.2014-10-14T10:04:07 INFO gdbserver/gdb-server.c: Target voltage is 3269 mV.2014-10-14T10:04:10 INFO src/stlink-common.c: Device connected is: F1 Medium-density device, id 0x200364102014-10-14T10:04:10 INFO src/stlink-common.c: SRAM size: 0x5000 bytes (20 KiB), Flash: 0x3fffc00 bytes (65535 KiB) in pages of 1024 bytes2014-10-14T10:04:10 INFO gdbserver/gdb-server.c: Chip ID is 00000410, Core ID is 1ba01477.2014-10-14T10:04:10 INFO gdbserver/gdb-server.c: Target voltage is 3264 mV.2014-10-14T10:04:44 INFO src/stlink-common.c: Device connected is: F1 Medium-density device, id 0x200364102014-10-14T10:04:44 INFO src/stlink-common.c: SRAM size: 0x5000 bytes (20 KiB), Flash: 0x2020000 bytes (32896 KiB) in pages of 1024 bytes2014-10-14T10:04:44 INFO gdbserver/gdb-server.c: Chip ID is 00000410, Core ID is 1ba01477.2014-10-14T10:04:44 INFO gdbserver/gdb-server.c: Target voltage is 3271 mV.Anyone got the same strange behaviour of this? I dont know where it belongs to.Greetings Michael #nucleo-f1032014-10-14 2:07 AM
Congrats for using the excellent st-link software from texane.
Run with -v90 switch to see more debug logs. By the way I did not clearly understood what is 'your' circuit, and how is the Nucleo connected to it, could you clarify ?2014-10-14 2:15 AM
2014-10-14 9:52 AM
Thats my board where i put the Nucleo on ->
And i tried it out with the verbose flag of the st-link util but it doesnt show more usefull information than without verbosing.So thats the new output with verbose flag:2014-10-14T18:44:55 DEBUG src/stlink-common.c: stlink current mode: debug (jtag or swd)
2014-10-14T18:44:55 DEBUG src/stlink-common.c: stlink current mode: debug (jtag or swd)
2014-10-14T18:44:55 INFO src/stlink-common.c: Loading device parameters....
2014-10-14T18:44:55 DEBUG src/stlink-common.c: *** stlink_core_id ***
2014-10-14T18:44:55 DEBUG src/stlink-common.c: core_id = 0x1ba01477
2014-10-14T18:44:55 DEBUG src/stlink-common.c: *** stlink_read_debug32 20036410 is 0xe0042000
2014-10-14T18:44:55 DEBUG src/stlink-common.c: *** stlink_read_debug32 ffff0080 is 0x1ffff7e0
2014-10-14T18:44:55 INFO src/stlink-common.c: Device connected is: F1 Medium-density device, id 0x20036410
2014-10-14T18:44:55 INFO src/stlink-common.c: SRAM size: 0x5000 bytes (20 KiB), Flash: 0x20000 bytes (128 KiB) in pages of 1024 bytes
2014-10-14T18:44:55 DEBUG src/stlink-common.c: *** looking up stlink version
2014-10-14T18:44:55 DEBUG src/stlink-common.c: st vid = 0x0483 (expect 0x0483)
2014-10-14T18:44:55 DEBUG src/stlink-common.c: stlink pid = 0x374b
2014-10-14T18:44:55 DEBUG src/stlink-common.c: stlink version = 0x2
2014-10-14T18:44:55 DEBUG src/stlink-common.c: jtag version = 0x13
2014-10-14T18:44:55 DEBUG src/stlink-common.c: swim version = 0x3
2014-10-14T18:44:55 DEBUG src/stlink-common.c: *** stlink_reset ***
2014-10-14T18:44:55 INFO gdbserver/gdb-server.c: Chip ID is 00000410, Core ID is 1ba01477.
2014-10-14T18:44:55 DEBUG src/stlink-common.c: *** reading target voltage
2014-10-14T18:44:55 DEBUG src/stlink-common.c: target voltage = 3271mV
2014-10-14T18:44:55 INFO gdbserver/gdb-server.c: Target voltage is 3271 mV.
2014-10-14T18:44:55 INFO gdbserver/gdb-server.c: Listening at *:4242...
^C2014-10-14T18:44:56 DEBUG src/stlink-common.c: *** stlink_run ***
2014-10-14T18:44:56 DEBUG src/stlink-common.c: *** stlink_exit_debug_mode ***
2014-10-14T18:44:56 DEBUG src/stlink-common.c: *** stlink_write_debug32 a05f0000 to 0xe000edf0
2014-10-14T18:44:56 DEBUG src/stlink-common.c: *** stlink_close ***2014-10-14T18:44:56 DEBUG src/stlink-common.c: stlink current mode: debug (jtag or swd)
2014-10-14T18:44:56 DEBUG src/stlink-common.c: stlink current mode: debug (jtag or swd)
2014-10-14T18:44:56 INFO src/stlink-common.c: Loading device parameters....
2014-10-14T18:44:56 DEBUG src/stlink-common.c: *** stlink_core_id ***
2014-10-14T18:44:56 DEBUG src/stlink-common.c: core_id = 0x1ba01477
2014-10-14T18:44:56 DEBUG src/stlink-common.c: *** stlink_read_debug32 20036410 is 0xe0042000
2014-10-14T18:44:56 DEBUG src/stlink-common.c: *** stlink_read_debug32 ffffffff is 0x1ffff7e0
2014-10-14T18:44:56 INFO src/stlink-common.c: Device connected is: F1 Medium-density device, id 0x20036410
2014-10-14T18:44:56 INFO src/stlink-common.c: SRAM size: 0x5000 bytes (20 KiB), Flash: 0x3fffc00 bytes (65535 KiB) in pages of 1024 bytes
2014-10-14T18:44:56 DEBUG src/stlink-common.c: *** looking up stlink version
2014-10-14T18:44:56 DEBUG src/stlink-common.c: st vid = 0x0483 (expect 0x0483)
2014-10-14T18:44:56 DEBUG src/stlink-common.c: stlink pid = 0x374b
2014-10-14T18:44:56 DEBUG src/stlink-common.c: stlink version = 0x2
2014-10-14T18:44:56 DEBUG src/stlink-common.c: jtag version = 0x13
2014-10-14T18:44:56 DEBUG src/stlink-common.c: swim version = 0x3
2014-10-14T18:44:56 DEBUG src/stlink-common.c: *** stlink_reset ***
2014-10-14T18:44:56 INFO gdbserver/gdb-server.c: Chip ID is 00000410, Core ID is 1ba01477.
2014-10-14T18:44:56 DEBUG src/stlink-common.c: *** reading target voltage
2014-10-14T18:44:56 DEBUG src/stlink-common.c: target voltage = 3263mV
2014-10-14T18:44:56 INFO gdbserver/gdb-server.c: Target voltage is 3263 mV.
2014-10-14T18:44:56 INFO gdbserver/gdb-server.c: Listening at *:4242...
^C2014-10-14T18:44:57 DEBUG src/stlink-common.c: *** stlink_run ***
2014-10-14T18:44:57 DEBUG src/stlink-common.c: *** stlink_exit_debug_mode ***
2014-10-14T18:44:57 DEBUG src/stlink-common.c: *** stlink_write_debug32 a05f0000 to 0xe000edf0
2014-10-14T18:44:57 DEBUG src/stlink-common.c: *** stlink_close ***
2014-10-14T18:45:34 DEBUG src/stlink-common.c: stlink current mode: debug (jtag or swd)
2014-10-14T18:45:34 DEBUG src/stlink-common.c: stlink current mode: debug (jtag or swd)
2014-10-14T18:45:34 INFO src/stlink-common.c: Loading device parameters....
2014-10-14T18:45:34 DEBUG src/stlink-common.c: *** stlink_core_id ***
2014-10-14T18:45:34 DEBUG src/stlink-common.c: core_id = 0x1ba01477
2014-10-14T18:45:34 DEBUG src/stlink-common.c: *** stlink_read_debug32 20036410 is 0xe0042000
2014-10-14T18:45:34 DEBUG src/stlink-common.c: *** stlink_read_debug32 ffff8080 is 0x1ffff7e0
2014-10-14T18:45:34 INFO src/stlink-common.c: Device connected is: F1 Medium-density device, id 0x20036410
2014-10-14T18:45:34 INFO src/stlink-common.c: SRAM size: 0x5000 bytes (20 KiB), Flash: 0x2020000 bytes (32896 KiB) in pages of 1024 bytes
2014-10-14T18:45:34 DEBUG src/stlink-common.c: *** looking up stlink version
2014-10-14T18:45:34 DEBUG src/stlink-common.c: st vid = 0x0483 (expect 0x0483)
2014-10-14T18:45:34 DEBUG src/stlink-common.c: stlink pid = 0x374b
2014-10-14T18:45:34 DEBUG src/stlink-common.c: stlink version = 0x2
2014-10-14T18:45:34 DEBUG src/stlink-common.c: jtag version = 0x13
2014-10-14T18:45:34 DEBUG src/stlink-common.c: swim version = 0x3
2014-10-14T18:45:34 DEBUG src/stlink-common.c: *** stlink_reset ***
2014-10-14T18:45:34 INFO gdbserver/gdb-server.c: Chip ID is 00000410, Core ID is 1ba01477.
2014-10-14T18:45:34 DEBUG src/stlink-common.c: *** reading target voltage
2014-10-14T18:45:34 DEBUG src/stlink-common.c: target voltage = 3264mV
2014-10-14T18:45:34 INFO gdbserver/gdb-server.c: Target voltage is 3264 mV.
2014-10-14T18:45:34 INFO gdbserver/gdb-server.c: Listening at *:4242...
But that dont tell me why the flash size jumps all around....?
2014-10-14 10:20 AM
Great.
Everything lies in the value read from register at 0x1ffff7e0, which is a 16-bit ''Flash size register'' according the RM. I this log it returned with 3 different values 0x80, 0xFFFF and 0x8080, among which the first one is the real one. I can't tell why this happen, but if I were you, I will try to connect to my board using windows base STLINK utility from ST, to check the stability of accessing the MCU through SWD. Is this possible that this happen because of a hardware conflict ? Does the Nucleo alone work normally ?2014-10-14 11:01 AM
At first on the breadboard prototype the Nucleo board worked perfectly but on the etched one the problems begun. After the second or third time i tried to flash the Nucleo board ontop of my etched board, the flashing starts to fail.
Now the strange flash size jumpings are there without my board also. The funny thing is that i sometimes when the flash size is randomly correct the flashing works. Also the verification is running correctly.2014-10-15 7:56 AM
Hi sauer.michael.002,
Do you have thesame
behavior
with ST-Link Utility
?
You can use the latest version of ST-LINK Utility available in the following link : Best Regards, Nouha2014-10-15 8:02 AM
Third party tools, probably broken. Contact the author of tools for support.
2014-10-16 10:59 AM
Hi,
i tried it now on a windows machine and what should i say... it works as expected. the only thing is that the core hangs in the while after setting pll as clock source.. could it be a problem with my external crystal?Greetings Michael2014-10-16 12:38 PM
JTAG/SWD generally requires a period of time for the debugger to break in and stop execution as it gains control. If you do things with the core that can potentially break access (WFI, DMA, Low Power, Clocks, Pins etc) early in the boot this will hamper the debugger, sometimes fatally. Resetting with BOOT0 High can remedy issues with user code.
Issues with PLLs and Clocks, double check suitable flash wait states prior to transitioning to faster sources.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.