2025-08-13 3:41 AM
hello,
i am working on project with a stm32wle5jc and am fairly new to stm tools. all was working well but after a little break on another project it will no longer flash the board with the stm ide (1.19.0) and says "No ST-LINK detected! Please connect ST-LINK and restart the debug session.". i have an st-link/v2 connected and the ide can actually see the st-link under "help" "st-link upgrade" (i am on a macbookpro m1, which also sees the st-link under "system report", "usb")
i can flash the code i want to flash from the ide (~/workspace/<projectname>/Debug/<projectname>.elf) with the stmcubeprogrammer without any problem
i have restarted the ide, restarted the mac, switched cables, switched projects, switch boards, tried a st board nucleo board with embedded st-link (or whatever it is)... but always get the same error message
what is going on?
any help greatly appreciated!
thanks, frank
Solved! Go to Solution.
2025-08-13 4:16 AM
finally! problem fixed.
found a post on stackoverflow which solved the problem by reinstalling st-link server
fixed the problem!
2025-08-13 4:16 AM
finally! problem fixed.
found a post on stackoverflow which solved the problem by reinstalling st-link server
fixed the problem!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.