2024-11-27 7:34 AM - last edited on 2024-11-27 7:50 AM by Andrew Neil
Good morning, I am trying to print a string on STM32F401RBT6 using vs code and Cmake, but I keep getting an issue, when I use '\n' the UART doesn't print nothing beyond the '\n', can somebody help me with this issue, please?
Solved! Go to Solution.
2024-11-27 7:43 AM - edited 2025-12-08 6:26 AM
@Gui_STM wrote:when I use '\n' the UART doesn't print nothing beyond the '\n',
I presume you mean, "doesn't print anything beyond the \n" ?
This is defined behaviour: the printf output is line-buffered; so the output is not sent until a line is complete - ie, until it reaches a \n
PS:
stderr is not buffered:
PPS:
Disable the buffering with:
setvbuf(stdout, NULL, _IONBF, 0);
#PrintfLineBuffered #StdoutLineBuffered #LineBuffered
2024-11-27 7:43 AM - edited 2025-12-08 6:26 AM
@Gui_STM wrote:when I use '\n' the UART doesn't print nothing beyond the '\n',
I presume you mean, "doesn't print anything beyond the \n" ?
This is defined behaviour: the printf output is line-buffered; so the output is not sent until a line is complete - ie, until it reaches a \n
PS:
stderr is not buffered:
PPS:
Disable the buffering with:
setvbuf(stdout, NULL, _IONBF, 0);
#PrintfLineBuffered #StdoutLineBuffered #LineBuffered
2024-11-27 8:20 AM
@Andrew Neil wrote:
printf output is line-buffered
To be more precise, the GCC default for stdout is line-buffered - so fprintf (or anything else) to stdout would, by default, show the same effect.
2024-11-27 8:42 AM
Or sprintf() into HAL_UART_Transmit(), it returns a length
2024-11-27 10:23 AM
Thank you, I will try this solution on my code.
2024-11-27 10:28 AM
But how does this solve my problem with printing on my UART?
2024-11-27 10:42 AM
@Gui_STM wrote:But how does this solve my problem with printing on my UART?
because your "problem" is due to the buffering performed by printf (strictly, by stdout).
By not using printf, you avoid that problem!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.