2017-01-11 6:47 AM
I am having some issues with CAN on my STM32F746 Disco board.
When I send the data as below, I get an error back...
CAN_IT_Status
=
HAL_CAN_Transmit_IT(
&
CanHandle
)
;
dum1
=
CanHandle
.
State
;
CANErrorCode
=
CanHandle
.
ErrorCode
;
so....
CAN_IT_STATUS=1, dum1=0x04, CANErrorCode=0.
on Probing through the HAL library, I can only assume that the CAN Mailboxes are not being cleared i.e. they are always full.
Does this sound like a hardware configuration thing as in the Message is never sent for some reason, or is there a bug in the library plenty of issues I can seen on this forum about CAN TX/TX Library problems.
If I probe the bus, with a scope there is absolutely nothing!
For info I am using the latest HAL libraries V1.5.
Here is my bus configuration:
void
HAL_CAN_MspInit(
CAN_HandleTypeDef*
hcan
)
{
GPIO_InitTypeDef
GPIO_InitStruct
;
/*##-1- Enable peripherals and GPIO Clocks #################################*/
/* Enable GPIO clock ****************************************/
CANx_GPIO_CLK_ENABLE
()
;
/* CAN1 Periph clock enable */
//CANx_CLK_ENABLE();
/*##-2- Configure peripheral GPIO ##########################################*/
/* CAN1 TX GPIO pin configuration */
GPIO_InitStruct
.
Pin
=
CANx_TX_PIN
;
GPIO_InitStruct
.
Mode
=
GPIO_MODE_AF_PP
;
GPIO_InitStruct
.
Speed
=
GPIO_SPEED_HIGH
;
GPIO_InitStruct
.
Pull
=
GPIO_NOPULL
;
GPIO_InitStruct
.
Alternate
=
CANx_TX_AF
;
HAL_GPIO_Init
(
CANx_TX_GPIO_PORT
,
&
GPIO_InitStruct
)
;
/* CAN1 RX GPIO pin configuration */
GPIO_InitStruct
.
Pin
=
CANx_RX_PIN
;
GPIO_InitStruct
.
Mode
=
GPIO_MODE_AF_PP
;
GPIO_InitStruct
.
Speed
=
GPIO_SPEED_HIGH
;
GPIO_InitStruct
.
Pull
=
GPIO_NOPULL
;
GPIO_InitStruct
.
Alternate
=
CANx_RX_AF
;
HAL_GPIO_Init
(
CANx_RX_GPIO_PORT
,
&
GPIO_InitStruct
)
;
}
And CAN Config:
void
CAN_Config(
void)
{
char
MyString
[
20
]
;
CAN_FilterConfTypeDef
sFilterConfig
;
HAL_CAN_DeInit
(
&
CanHandle
)
;
//De-Init first
//HAL_CAN_DeInit(&CanHandle);
/* CAN1 Periph clock enable */
CANx_CLK_ENABLE
()
;
/*##-1- Configure the CAN peripheral #######################################*/
CanHandle
.
Instance
=
CANx
;
 
CanHandle
.
pTxMsg
=
&
TxMessage
;
CanHandle
.
pRxMsg
=
&
RxMessage
;
//Calculation is CANCLK/(BRP*(BS1+BS2+1)) = 50/5*(7+2+1) = 1
CanHandle
.
Init
.
TTCM
=
DISABLE;
CanHandle
.
Init
.
ABOM
=
ENABLE;
CanHandle
.
Init
.
AWUM
=
DISABLE;
CanHandle
.
Init
.
NART
=
DISABLE;
CanHandle
.
Init
.
RFLM
=
DISABLE;
CanHandle
.
Init
.
TXFP
=
DISABLE;
CanHandle
.
Init
.
Mode
=
CAN_MODE_NORMAL
;
CanHandle
.
Init
.
SJW
=
CAN_SJW_1TQ
;
//1MBit
CanHandle
.
Init
.
BS1
=
CAN_BS1_7TQ
;
//Aim for between 70% & 85% Bit sampling point
CanHandle
.
Init
.
BS2
=
CAN_BS2_2TQ
;
//
CanHandle
.
Init
.
Prescaler
=
5
;
//2;//?
CanHandle
.
pTxMsg
->
StdId
=
0x321
;
CanHandle
.
pTxMsg
->
ExtId
=
0x1111
;
CanHandle
.
pTxMsg
->
RTR
=
CAN_RTR_DATA
;
CanHandle
.
pTxMsg
->
IDE
=
CAN_ID_STD
;
CanHandle
.
pTxMsg
->
DLC
=
8
;
CanHandle
.
pTxMsg
->
Data
[
0
]
=
0x00
;
CanHandle
.
pTxMsg
->
Data
[
1
]
=
0x01
;
 
if
(
HAL_CAN_Init(
&
CanHandle
)
!=
HAL_OK)
{
/* Initialization Error */
Error_Handler
()
;
}
/*##-2- Configure the CAN Filter ###########################################*/
sFilterConfig
.
FilterNumber
=
0
;
sFilterConfig
.
FilterMode
=
CAN_FILTERMODE_IDMASK
;
sFilterConfig
.
FilterScale
=
CAN_FILTERSCALE_32BIT
;
sFilterConfig
.
FilterIdHigh
=
0x0000
;
sFilterConfig
.
FilterIdLow
=
0x0000
;
sFilterConfig
.
FilterMaskIdHigh
=
0x0000
;
sFilterConfig
.
FilterMaskIdLow
=
0x0000
;
sFilterConfig
.
FilterFIFOAssignment
=
0
;
sFilterConfig
.
FilterActivation
=
ENABLE;
sFilterConfig
.
BankNumber
=
14
;
if
(
HAL_CAN_ConfigFilter(
&
CanHandle
,
&
sFilterConfig
)
!=
HAL_OK)
{
/* Filter configuration Error */
Error_Handler
()
;
}
}
2017-01-12 1:57 AM
Stand down, I have got my PB8/PB9 pins the wrong way around on the schematic!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.