STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32 dual core booting sequences

Hello ST Community,I read in the follow post question about boot sequences for STM32:STM32H7 dual core: How to start with a busy-waitin... - STMicroelectronics CommunitySo, in the post above, I see that is explain the first three Boot order of the Ta...

Table_8_RM0399.png

Resolved! Query about data coming out of STM32N6570-DK MCU

I am using ADC + DMA + USART1 + Timer in STM32 IDE in a setup consisting of:Motor → Sensors → MCU (STM32N6) → PCI am capturing the signal received at the serial port using NanoEdge AI. I have shared screenshots of:The actual current waveform observed...

AndrewNeil_0-1771330500890.jpeg AndrewNeil_1-1771330518452.jpeg

Resolved! ADC + GPDMA output values are incorrect

I am using STM32H563 and using seven pins to read data, all through ADC1 with GPDMA1 Channel0 -2 Words internal FIFO. I connected all seven pins to ground, expecting to get all zeros or values close to zero, but the readings seem to fluctuate randoml...

Hueiyi_0-1770884386090.png Hueiyi_1-1770884486376.png Hueiyi_2-1770884580706.png Hueiyi_3-1770884707319.png
Hueiyi by Associate II
  • 294 Views
  • 2 replies
  • 0 kudos

Resolved! N6 PLL: FRAC change on the fly as in H7 impossible ?

Heyho,the title says it...In RM0486, 14.6.5 PLL description, page 437 / 438 I find this:Using the PLLs in fractional modePLL off ... set FRAC ... PLL onCaution: Do not update DIVN and DIVNFRAC after the PLL has been enabled.On the other hand, there a...

LCE by Principal II
  • 287 Views
  • 2 replies
  • 0 kudos

Resolved! USB issues with STM32F103C8T6

Hello, I made a board with an STM32F103C8T6 which uses USB.My issue is that when conecting USB (self powered or with external power) I get the following error on windows:Windows has stopped this device because it has reported problems. (Code 43) A r...

USB_sch.png MCU_sch.png USB_layout.png

Resolved! SDRAM Option Missing for STM32H7A3ZIT6Q in CubeIDE

Hi,I selected STM32H7A3ZIT6Q to use external SDRAM. However, in STM32CubeIDE under Connectivity → FMC, the SDRAM option is not available.When I select STM32H7A3ZIT6 (non-Q), the SDRAM option appears.Does the STM32H7A3ZIT6Q support SDRAM, or is this a...

Ashad27 by Associate
  • 245 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.