2019-07-06 9:54 AM
Im debugging with an ST-LINK J9357 debugger chip in Eclipse's debug workbench . I've been over the debug configurations many times and cannot find an error. Once i start the debug and it shuts off the connection there isn't even an error box detailing the error.
The console tab displays the following after cutting off:
GNU MCU Eclipse 32-bits Open On-Chip Debugger 0.10.0+dev-00254-g2ec04e4e (2017-11-10-11:53)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
Info : auto-selecting first available session transport "hla_swd". To override use 'transport select <transport>'.
Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD
adapter speed: 1000 kHz
adapter_nsrst_delay: 100
none separate
Started by GNU MCU Eclipse
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : Unable to match requested speed 1000 kHz, using 950 kHz
Info : Unable to match requested speed 1000 kHz, using 950 kHz
Info : clock speed 950 kHz
Info : STLINK v2 JTAG v24 API v2 SWIM v0 VID 0x0483 PID 0x3748
Info : using stlink api v2
Info : Target voltage: 3.237042
Info : stm32f0x.cpu: hardware has 4 breakpoints, 2 watchpoints
Info : Listening on port 3333 for gdb connections
2019-07-06 11:31 AM
Sorry not familiar with the J9357 device. v24 is rather an old firmware, consider updating it to something more recent, and using software/drivers that aren't 2 years old.
Connectivity can drop for an number of reasons, primarily you reconfiguring the pins involved with the SWD connection, and powering down the circuits the debugger is using, ie low power modes and WFI instructions.
You might try better tools, and see if they work more effectively. Keil for example has free licensing for STM32 CM0(+) parts.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.