2019-07-06 6:16 AM
Hello everyone,
I am trying to interface my STM32F401RE with OV7670 camera. I have set the input clock for the camera from the MCO output of the board at 8MHz. Because my board is not provided with DCMI, I have to explicitly implement the communication protocol of the camera. Apparently I am able to get an image, but it seems more noise than real data. I send the data from the MCU to my PC via UART to check the image with an external software, which is working if I test it with predefined values (eg sending always zero from MCU results in a full black image). The camera registers also seem correctly set , just looking at their content after writing. I suspect about subtle timing problems that prevent me from getting the image. I retrieve the 8 bits of data from the camera by reading the GPIOx IDR register.
Here is the code involved in reading the image.
while (!(HAL_GPIO_ReadPin(GPIOA, GPIO_PIN_11) == GPIO_PIN_SET)); //wait for high VSYNC
while ((HAL_GPIO_ReadPin(GPIOA, GPIO_PIN_11) == GPIO_PIN_SET)); //wait for low VSYNC
y = height;
while (y--){
x = width;
while (x--){
while ((HAL_GPIO_ReadPin(GPIOA, GPIO_PIN_9) == GPIO_PIN_SET)); //wait for low PCLK
data = (uint16_t)GPIOB->IDR & 0x00ff; // read port B to get input from camera
effective_data = (uint8_t)data; // only the last 8 bits contain my data
HAL_UART_Transmit(&huart2, (uint8_t *)effective_data, 1, 10);
data = 0;
effective_data = 0;
while (!(HAL_GPIO_ReadPin(GPIOA, GPIO_PIN_9) == GPIO_PIN_SET)); //wait for high PCLK
while ((HAL_GPIO_ReadPin(GPIOA, GPIO_PIN_9) == GPIO_PIN_SET)); //wait for low PCLK
while (!(HAL_GPIO_ReadPin(GPIOA, GPIO_PIN_9) == GPIO_PIN_SET));//wait for high PCLK
}
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.