2014-07-14 3:19 AM
Hello,
I have a trouble with my DAC, for example when I set the DAC output (Channel1 orChannel2) to the maximum voltage, the DAC generate the minimum voltage:DAC_SetChannel1Data(DAC_Align_12b_R, 4095); Vout
~
0VDAC_SetChannel1Data(DAC_Align_12b_R, 0); Vout
~
3.3VDAC_SetChannel1Data(DAC_Align_12b_R, 1000); Vout
~
0.8V The strange thing is, I have two test boards, and the problem happens only on one board. The other board have a correct behavior, with the same project! Do you have any ideas? Thanks a lot!DAC_SetChannel1Data(DAC_Align_12b_R, 4095); Vout
~
0VDAC_SetChannel1Data(DAC_Align_12b_R, 4095); Vout
~
0V #whiskey-tango-foxtrot #oscar-mike-golf2015-06-02 4:23 AM
Hi,
Me too. I have built around 10 boards with exact same configuration and 30 other boards using same design for DAC part after that but it never appeared.2015-06-03 7:11 AM
Yes it sounds totally right :) I think I made a mistake with this line...
2015-06-03 10:07 AM
If you still have the faulty board, could you please repeat the experiment and report back for the voltages for DAC set to say 0, 1000, 2000, 3000, 4096?
JW2015-06-12 6:50 AM
I'm sorry but I don't have this board anymore... But i'm 100% sure that the voltages was perfectly inverted from 3.3V to 0V.
2016-02-29 1:49 AM
I ran into the very same problem. My board outputted the correct voltages until I lend it out to a colleague for some testing. He noticed the inverted values which made us search for the problem.
By disabling the output buffer of the DAC, the ouput values are correct but this isn't desirable for our project. We believe a short on the output pin blew some of the internal hardware of the output buffer. After replacing the MCU the output values were correct again with the output buffer enabled.Don't know whether this is of any help for you by now but just wanted to share the info so others don't have to spend an entire afternoon looking for something wrong in the code when the hardware was faulty.Cheers!2018-06-22 3:29 AM
You must disable the output buffer
in function MX_DAC_Init
sConfig.DAC_OutputBuffer = DAC_OUTPUTBUFFER_DISABLE;
2018-06-23 10:37 AM
Hi ,
That issue is a physical damage of the DAC pad ( PA4 or PA5) due that all board VDD flowed thru that pad and exceeding our Maxium Rating. The destroyed path is the one going to our Analog rail thru the activation of the output buffer. This is not normal behavior and you should replace your destroyed MCU due to EOS.
Ciao,
STOne-32
2024-07-30 10:15 PM - edited 2024-07-30 10:17 PM
hello,
I have this similar problem but only for one channel.
Channel 1 -- Connected to PA4 pin gives the inverted output , but the Channel 2 -- connected to PA5 pin give correct output.
Currently I have only one board for testing.
So if the DAC is damaged , than this should be seen for both Channels right?
2024-07-31 11:53 PM
> So if the DAC is damaged , than this should be seen for both Channels right?
No.
The output buffers for the two channels are independent from each other, so you probably have one of them damaged.
JW
2024-10-21 9:01 PM
Is your DAC driving in buffered mode (non-inverting) or unbuffered mode driving a virtual earth inverting opamp (inverting). Obviously this would explain it depending on your choice.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.