2024-12-11 11:29 PM - edited 2024-12-11 11:30 PM
On an STM32F103CB I'm running the USB Custom HID Device STM32CubeIDE example.
It has 1 USB HID Interface with 2 USB Endpoints (Input and Output, interrupt transfers), and I've added a Report Descriptor with several top-level collections, and it's working well.
I need to add 1 more Interface with a single HID interrupt Endpoint (Input (device-to-host), interrupt transfers).
I've modified the Interface Descriptor inside the Configuration Descriptor `USBD_CUSTOM_HID_CfgFSDesc` in `usbd_customhid.c`, and I've also added an extra Endpoint descriptor (though I'm not sure it's correct):
// ----------------------------------------------------------------------
// byte 0
0x09, // bLength: Configuration Descriptor size
USB_DESC_TYPE_CONFIGURATION, // bDescriptorType: Configuration Descriptor typee
USB_CUSTOM_HID_CONFIG_DESC_SIZ,
// wTotalLength: Bytes returned
0x00,
0x01/*0x02 0x03*/, // bNumInterfaces: 1 interface
0x01, // bConfigurationValue: configuration value
0x00, // iConfiguration: index of string descriptor describing the configuration
0xc0, // bmAttributes: bus powered
0x32, // MaxPower 100 mA: this current is used for detecting Vbus
// ----------------------------------------------------------------------
// ---------------------------------------------------------------------- 0.0) interface 0 (CUSTOM_HID): Interface Descriptor?
// byte 9
0x09, // bLength: Interface Descriptor size
USB_DESC_TYPE_INTERFACE, // bDescriptorType: Interface Descriptor type
0x00, // bInterfaceNumber: interface 0x00?
0x00, // bAlternateSetting: alternate setting
0x02, // bNumEndpoints
0x03, // bInterfaceClass: CUSTOM_HID
0x00, // bInterfaceSubClass: 0=no boot, 1=BOOT
0x00, // nInterfaceProtocol: 0=none, 1=keyboard, 2=mouse
0x00, // iInterface: index of string descriptor
// ---------------------------------------------------------------------- 0.1) interface 0 (CUSTOM_HID): Report-Descriptor Descriptor?
// byte 18
0x09, // bLength: CUSTOM_HID Descriptor size
CUSTOM_HID_DESCRIPTOR_TYPE, // bDescriptorType: CUSTOM_HID Descriptor type
0x11, // bCUSTOM_HIDUSTOM_HID: CUSTOM_HID Class Spec release number
0x01,
0x00, // bCountryCode: hardware target country
0x01, // bNumDescriptors: number of CUSTOM_HID class descriptors to follow
0x22, // bDescriptorType
LOBYTE(USBD_CUSTOM_HID_REPORT_DESC_SIZE), // wItemLength: total length of Report Descriptor
HIBYTE(USBD_CUSTOM_HID_REPORT_DESC_SIZE), // wItemLength: total length of Report Descriptor
// ---------------------------------------------------------------------- 0.2.0) interface 0 (CUSTOM_HID): Endpoint Descriptor?: endpoint 0
// byte 27
0x07, // bLength: Endpoint Descriptor size
USB_DESC_TYPE_ENDPOINT, // bDescriptorType: Endpoint Descriptor type
CUSTOM_HID_EPIN_ADDR, // bEndpointAddress: endpoint address (IN)
0x03, // bmAttributes: interrupt endpoint
CUSTOM_HID_EPIN_SIZE, // wMaxPacketSize: 2 byte max
0x00,
CUSTOM_HID_FS_BINTERVAL, // bInterval: polling interval
// ---------------------------------------------------------------------- 0.2.1) interface 0 (CUSTOM_HID): Endpoint Descriptor?: endpoint 1
// byte 34
0x07, // bLength: Endpoint Descriptor size
USB_DESC_TYPE_ENDPOINT, // bDescriptorType: Endpoint Descriptor type
CUSTOM_HID_EPOUT_ADDR, // bEndpointAddress: endpoint address (OUT)
0x03, // bmAttributes: interrupt endpoint
CUSTOM_HID_EPOUT_SIZE, // wMaxPacketSize: 2 bytes max
0x00,
CUSTOM_HID_FS_BINTERVAL, // bInterval: polling interval
// ----------------------------------------------------------------------
// ---------------------------------------------------------------------- 1.0) interface 1: Interface Descriptor?: for boot keyboard
// byte 41
0x09, // bLength
USB_DESC_TYPE_INTERFACE, // bDescriptorType
0x01, // bInterfaceNumber: interface 0x01?
0x00, // bAlternateSetting: 0
0x01, // bNumEndpoints
0x03, // bInterfaceClass: CUSTOM_HID
0x00, // bInterfaceSubClass: 0=no boot, 1=BOOT
0x01, // nInterfaceProtocol: 0=none, 1=keyboard, 2=mouse
0x00, // iInterface
// ---------------------------------------------------------------------- 1.1) interface 1: Report-Descriptor Descriptor?
0x09, // bLength
CUSTOM_HID_DESCRIPTOR_TYPE, // bDescriptorType
0x11, // bCUSTOM_HID version
0x01,
0x00, // bCountryCode
0x01, // bNumDescriptors
0x22, // bDescriptorType: Report
LOBYTE(HID_IF1_IRP_DESC_BDIM), // wItemLength
HIBYTE(HID_IF1_IRP_DESC_BDIM), // wItemLength
// ---------------------------------------------------------------------- 1.2.0) interface 1: Endpoint Descriptor?: endpoint 0
0x07, // bLength
USB_DESC_TYPE_ENDPOINT, // bDescriptorType: Endpoint Descriptor type
CUSTOM_HID_EPIN2_ADDR, // bEndpointAddress
0x03, // bmAttributes: interrupt endpoint
CUSTOM_HID_EPIN2_SIZE, // wMaxPacketSize
0x00,
CUSTOM_HID_FS_BINTERVAL, // bInterval
My question (other than: Is the Configuration Descriptor correct?) is: what other changes do I need to make to the STM32CubeIDE example & USB stack to make it work with 2 (HID) interfaces?
2024-12-11 11:48 PM
You need to modify the class request handler for GET_HID_DESCRIPTOR. It should check the interface number and, based on that, return one or another HID descriptor. Then you need to add the handling for endpoint traffic.
2024-12-12 2:24 AM
I suggest you register composite class. Register two instances of HID class. You do not need to update the configuration descriptor to register two instances. See this example for dual CDC interfaces as an example How to implement a dual CDC ACM USB device using t... - STMicroelectronics Community
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.