2018-04-18 3:00 AM
Hi to all,
I'm working with an SPWF04 wifi module linked on NUCLEO F411RE board, using MQTT protocol; all works perfectly but I'm wondering if there is a maximum length (in byte) for a MQTT published message. So, when I use the AT command:
AT+S.MQTTPUB=0,<topic>,[<QoS>],[<retained_flag>],<len><cr>{data}
what is the maximum length in byte of {data} ? I use the UART interface for communicate with wifi module, so I think there is in the module a buffer for this UART, and so it's impossible to send messages over a certain byte numbers...
Please, could anyone tell me if there is a really maximum data length ?
Regards
Davide Urbano
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.