2017-04-06 11:25 AM
Hi!
I have a question regarding the stm32f0 DMA engine. I am using an stm32f0discovery MB1034B evaluation board.
I have the following setup:
The SPI dma is configured to transmit 3 bytes from memory to the spi peripheral. Let's say I transfer bytes 0x0A 0x0B 0x0C.
If I trigger the dma transfer via the spi tx dma en flag i cann see my three bytes on the spi bus (0x0a 0x0b 0x0c).
Then the DMA transfer completet isr fires. All fine.
Now i want to trigger the dma transfer by a timer1 ch2 compare match (which is as well on dma1 channel 3).
The thing is I can only see single byte transfers. On cc match number one I see 0x0a.
One second later (on the second compare match) I see 0x0b. Another second later I see 0x0c.
Then the DMA transfer completet isr fires.
Why does the timer only initiate single transfers? I expected to see the same transfer as when triggering the spi manually?!
Any hints?
2017-04-07 2:15 AM
That's how DMA works: one trigger (request), one transfer.
If you trigger DMA from SPI_Tx, there is one transfer every time the SPI_SR.TXE flag goes high. As the data written to SPI_DR are transferred to the shift register when it is/gets empty, there's one such trigger each time this transferr happens.
If you trigger it from timer, there's one transfer every time the compare happens.
JW
2017-04-07 10:39 AM
Ah now I understand. I was not aware that the SPI txe flag retriggers the dma for all following bytes.
That makes perfectly sense now, thanks!
2017-04-10 1:36 PM
Is there a way to start a multi-byte spi dma from a compare match? That way I would not have any issues with the interrupt latency.
2017-04-10 7:38 PM
Real problem there is aligning the TIM pulses with the transmit buffer being empty.
You might be able to use an advanced timer in repetition mode to fire CCx 3 times.
Consider an FPGA/CPLD with a 24-bit shift register triggered by whatever event it is you want to align against. Or generate SPI clocks for a slave feed via a DMA buffer/loop
2017-04-10 11:25 PM
Real problem there is aligning the TIM pulses with the transmit buffer being empty.
Not that of a problem in case of master SPI, unless you insist the clock being perectly continuous. Both the SPI a Timer work out of a common clock source so things are perfectly synchronous.
You might be able to use an advanced timer in repetition mode to fire CCx 3 times.
+1
Alternatively, at a cost of 2 DMA channels you can fill a 'conventional' SPI-triggered DMA's control register by a TIM-triggered DMA.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.