2013-07-05 3:02 AM
hello
i have usb <-> R232 converter and i want to make it receive correct characters from stm32f4 board , so which capacitors i have to use with max232 to realise this ? and thnx :)2013-07-05 7:50 AM
What does the part documentation tell you about the voltages and capacitors?
2013-07-05 8:43 AM
i posted in other forum and many answered that u can control output voltage by changing the value of capacitors . so if it's wrong , can u propose for me a solution ?
2013-07-05 10:56 AM
You can use anyone between 100nF ~ 1uF. It can be changed with the distance and the amount the noise of enviroment. Only be carefull, MAX232 need a voltage supply of 4.5V to 5.5V and most stm32 boards are using 3.3V regulator. Maybe will be better use a MAX3232 that support a voltage supply of 3V to 5.5V.
2013-07-05 11:03 AM
thnx so did u tried before that marge of capacitors values 100nF ~ 1uF with max232 to interface stm32f4 and and pc via usb <-> r232 adapter ?
2013-07-05 11:09 AM
Because generally they meant by it the level +/-12v for the rs232 <-> r232 cable
2013-07-05 12:12 PM
The MAX3232 w/0.1uF parts at 3.3V is much more likely to have outputs closer to +/-6V, which would meet EIA/TIA-232-F and EIA/TIA-562
http://pdfserv.maximintegrated.com/en/ds/MAX3222-MAX3241.pdf
If you read the documentation you'd be able to do the design work yourself, rather than ask questions that demonstrate you haven't.2013-07-05 12:51 PM
thank you clive i hope it will work :)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.