2016-07-14 8:27 AM
I'm using an STM32L151 board and I want to know how to map a memory address to its function. For example:
LDR.W R0, =0x20002A20
MOVS R2, #4
MOVS R1, #4
STR R1, [R0,#0x14]
LDR.W R1, =0x20002224
STR.W R2, [R1,#0x1B8] In a rough translation to pseudocode, we see that:
R0 = *(0x20002A20)
R1 = 4
R2 = 4
The 4 bit is set to one on memory address of R0 + 0x14
R1 = *(0x20002224)
The 4 bit is set to one on memory address of R1 + 0x1B8 But I am having a hard time figuring out what the code is actually doing. I know it is in the SRAM (according to the memory map) but I cannot find the 0x2A20 or 0x2224 address offset does. I've been looking in the header files (like stm32l151xc.h) and cannot find anything. Once I know how to find what these addresses map to, I can see what setting the 4 bit to ''on'' does. How do I find what 0x2A20 and 0x2224 map to? Where should I
2016-07-14 9:40 AM
It is not going to be in the manuals or include files.
The address comes from where the linker places specific variables you have allocated, mostly on a first come first served basis. You can review the symbols exported by the linker in the .MAP file (or within the .AXF/.EXF object). For structures or arrays you might only get the address of the base, and the length, and you'd have to figure if the address falls within that.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.