2023-11-15 2:42 AM
Hi,
I'm using on a STM32L4R9 a LPTimer1 in interrupt mode. If i use it with the PCLK1, HSI or LSI as clocksource it works as expected. It counts to the ARR value and then the interrupt occours. If i use the LSE as clocksource the LPTimer seems only to count to 1 and the interrupt happens way to often (propably also at 1).
The LSE is also used for the RTC, which works fine.
Solved! Go to Solution.
2023-11-22 4:41 AM
Of course not. I completely overlooked it. Probably because I didn't expect that the compiler wouldn't have an error here.
Thank you
Felix
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.