2019-06-04 7:44 AM
I develop an own LIN slave node software stack for the STM32F103RB. This stack has to pass all tests from the LIN Conformance Test (according to ISO 17987-6). This test is a customer requirement.
Actually the software and/or the hardware could not detect error in the stop bits. (See test case PT-CT 38).
Is there a solution to detect a stop bit error during receiving or transmitting a data byte?
I could not find such a flag in the reference manual (RM0008).
Is there an undocumented feature to solve this problem?
2019-06-18 3:19 AM
Hello @fehrlest ,
Please note that STM32 devices are general purpose MCUs not dedicated for automotive usage.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.