2023-12-12 10:54 AM
Dear all,
I am new to STM32 development environment. I recently purchases STM32F407G-DISC1. I also purchased mini USB cable. When I connected the board to the PC, I can see that LD1 is on (RED). I can upgrade the driver for ST-Link as well. So, I am assuming there is connection established between board and the PC. Then, I write the first piece of code as attached below to see the LED blinks. It compiles very well. However, the code is not downloaded to the board. When I click on debug, it stucks at Launching: Initializing debugger services. It does not complete the progress. Please see the attachment2. I am helpless on this and require immediate support. I really liked the board and dont want to lose the enthusisasim.
Thank you.
2023-12-12 11:53 AM - edited 2023-12-12 11:54 AM
Hello @demir and welcome to the ST Community :smiling_face_with_smiling_eyes:.
Since the LD1 is on RED that means the communication between the ST-LINK/V2-A of the board and the PC is not established.
I suggest you to check your usb cable (try using another one) . Also, try to use another USB port for the communication.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-12-12 12:53 PM
Thank you for the answer.
I have changed the USB port but the issue persists. I am using this cable (MP01787), do you think this is not the proper one ? Could you please suggest me the right cable ?
2023-12-12 10:32 PM
Can you try to connect your board to another PC.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-12-12 10:44 PM
2023-12-12 11:10 PM
can you try to connect your board to STM32CubeProgrammer and do a full chip erase.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-12-12 11:55 PM
I installed cubeprogrammer and performed full chip erase. Now, I can see that LD1 is green so that means I can communicate to the board, right ? Afterwards, I opened STM32 CUBEIDE, wrote a simple program to check LED3(Orange) blinks or not. I clicked on debug--> debug as applicatiom. The code is not downloaded to the board. Again, it is stuck at launching: initializing debugger services. Please see the attached images.
Thanks.
2023-12-13 12:18 AM
Lets try a few things:
Right click the project in the project explorer and select "Index -> Rebuild"
Make a clean build by right clicking the project and select "Clean Project"
Then build the project again
If none of the two steps above helps, try making a new workspace and import the project to the new workspace and see if anything changes
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-12-13 3:13 AM - edited 2023-12-13 3:34 AM
Thats unfortunate. I tried all steps above, it didnt work at all.
Also, when I intended to cancel debug operation, it is not responding at all.
I have also updated the driver for ST-Link.
After the firmware update LD1 comm went back to red again. It was green before after full chip erase.
Please note that, I have performed full chip erase again, then I noticed that LD1 blinks red and green, then stops at green for a second or less, then this pattern continued until I closed STM Cube Programmer. When I closed cube programmer, LD1 turned to stable greed light.
2023-12-13 5:28 AM
Are you using the last version of the STM32CubeIDE - Integrated Development Environment for STM32 - STMicroelectronics. If no, I suggest you migrate to the last version.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.