2025-03-24 3:06 AM - edited 2025-03-25 6:24 AM
Hi,
I am working on the SBSFU default code, which handles swapping content from the download slot to the active slot. However, I need to skip the swapping process and after Decryption download slot boot directly from the download slot.
Could you please guide me on how to boot directly from the download slot?
please find the attached flowchart for reference.
Regards,
Raja
I have made changes in the SFU_BOOT_SM_ExecuteUserFw state and after application is not launching after changes
static void SFU_BOOT_SM_ExecuteUserFw(void)
{
SFU_ErrorStatus e_ret_status = SFU_ERROR;
SE_StatusTypeDef e_se_status = SE_KO;
uint32_t i;
TRACE("\r\n= [SBOOT] STATE: EXECUTE USER FIRMWARE");
/* Reload Watchdog */
(void) SFU_LL_SECU_IWDG_Refresh();
/* Verify if authentication and integrity controls performed at SFU_STATE_VERIFY_USER_FW_SIGNATURE */
FLOW_CONTROL_CHECK(uFlowCryptoValue, FLOW_CTRL_INTEGRITY);
for (i = 0U; i < SFU_NB_MAX_ACTIVE_IMAGE; i++)
{
/* Slot configured ? */
if(SlotStartAdd[SLOT_DWL_1 + i] != 0U) //if(SlotStartAdd[SLOT_ACTIVE_1 + i] != 0U)
{
/* FW installed ? */
if (SFU_SUCCESS == SFU_IMG_DetectFW(SLOT_DWL_1 + i)) //if(SFU_SUCCESS == SFU_IMG_DetectFW(SLOT_ACTIVE_1 + i))
{
/* Initialize Flow control */
FLOW_CONTROL_INIT(uFlowCryptoValue, FLOW_CTRL_INIT_VALUE);
/* Check the header signature */
if (SFU_IMG_VerifyActiveImgMetadata(SLOT_DWL_1 + i) != SFU_SUCCESS) // if (SFU_IMG_VerifyActiveImgMetadata(SLOT_ACTIVE_1 + i) != SFU_SUCCESS)
{
/* Security issue : execution stopped ! */
SFU_EXCPT_Security_Error();
}
/* Check the FW signature */
if (SFU_IMG_ControlActiveImgTag(SLOT_DWL_1 + i) != SFU_SUCCESS) // if (SFU_IMG_ControlActiveImgTag(SLOT_ACTIVE_1 + i) != SFU_SUCCESS)
{
/* Security issue : execution stopped ! */
SFU_EXCPT_Security_Error();
}
#if defined(ENABLE_IMAGE_STATE_HANDLING) && !defined(SFU_NO_SWAP)
/* Move the state to SELFTEST for the new images */
if (SFU_IMG_UpdateImageState(SLOT_ACTIVE_1 + i) != SFU_SUCCESS)
{
/* Image state cannot be changed : What to do ?
==> decision to continue execution */
TRACE("\r\n= [FWIMG] WARNING: IMAGE STATE CANNOT BE CHANGED!");
}
#endif /* ENABLE_IMAGE_STATE_HANDLING && !(SFU_NO_SWAP) */
/* Verify if authentication and integrity controls performed */
FLOW_CONTROL_CHECK(uFlowCryptoValue, FLOW_CTRL_INTEGRITY);
}
}
}
m_ActiveSlotToExecute = SLOT_DWL_1; // Hard coding m_ActiveSlotToExecute variable to boot from download slot
// boot from download slot when new firmware is installed
#endif
/*
* You may decide to implement additional checks before running the Firmware.
* For the time being we launch the FW present in the active slot.
*
* The bootloader must also take care of the security aspects:
* A.configure (if any) the external flash in execution mode with On The Fly DECryption (OTFDEC)
* B.lock the SE services the UserApp is not allowed to call
* C.leave secure boot mode
*/
/* Configure active slot in execution mode with OTFDEC (if any) : required in case of external flash */
TRACE("\r\nActiveSlotToExecute=%u\r\n",m_ActiveSlotToExecute);
e_ret_status = SFU_LL_FLASH_Config_Exe(m_ActiveSlotToExecute);
if (e_ret_status != SFU_SUCCESS)
{
/* Set the error before forcing a reboot, don't care of return value as followed by reboot */
SFU_EXCPT_SetError(SFU_EXCPT_FLASH_CFG_ERR);
/* This is the last operation executed. Force a System Reset */
SFU_BOOT_ForceReboot();
}
if (e_ret_status == SFU_SUCCESS)
{
/* Lock part of Secure Engine services */
if (SE_LockRestrictServices(&e_se_status) == SE_SUCCESS)
{
/* Double instruction to avoid basic fault injection */
if (SE_LockRestrictServices(&e_se_status) == SE_SUCCESS)
{
/* De-initialize the SB_SFU bootloader before launching the UserApp */
(void)SFU_BOOT_DeInit(); /* the return value is not checked, we will always try launching the UserApp */
/* Last flow control : lock service */
FLOW_CONTROL_STEP(uFlowCryptoValue, FLOW_STEP_LOCK_SERVICE, FLOW_CTRL_LOCK_SERVICE);
/* This function should not return */
e_ret_status = SFU_IMG_LaunchActiveImg(m_ActiveSlotToExecute);
}
2025-03-27 10:34 PM - edited 2025-03-27 10:34 PM
Hi Team,
Still there is no response.
Regards,
Raja
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.