2018-02-18 4:34 AM
2018-02-18 6:11 AM
Have you loaded the F1 packs?
2018-02-18 6:23 AM
Since you want to use CubeMX isn't be easier to start the project from the CubeMX, enable resources (GPIO, etc) and generate project for Keil. Then start Keil project - the uvision will download all the required packages...
2018-02-18 7:31 AM
yes i did
2018-02-19 5:58 AM
i did that !!!
2018-04-18 1:28 AM
Hi Mohammed,
unfortunately Keil
claims that's only STM32F2, STM32F4, and STM32F7 have the support for STM32CubeMX in their software packs, the STM32F1 is not yet supported.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.