STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F407VG Discovery + M24SR

Posted on April 18, 2018 at 11:18   Hello everyone, I'm trying to connect M24SR to the microprocessor STM32fF407.   Previously used the STM32fF107VC processor, and a slightly corrected demo version of the software for the M24SR Discovery, everything...

STM32F446RE - PGSERR & PGPERR raised

Posted on April 18, 2018 at 09:59Hi, I'm working on a project and the code works very well (stable, no crash...). But recently I decided to add EEPROM emulation and therefore started to add some code and test. I realized the emulation wasn't working...

Keil -- STM32cubemx -- Stm32f103

Posted on February 18, 2018 at 13:34hi ..when i create new Project in keil (the device is stm32f103c6)  i cant find the Option in the photo below ..can anyone help plz .. 

Moha-Affa by Associate II
  • 2827 Views
  • 5 replies
  • 0 kudos

Resolved! STM32F417VET - FSMC memory

Posted on April 17, 2018 at 12:54Hi,I have a STM32F417 processor and I would like to use the FSMC module with an LCD (ILI9481).The used pins: NE1 and the RS pin of LCD connected to A25.The bank of the memory is clear that if I use the NE1 then I hav...

stm32l0 systick handler with internal osc.

Posted on April 18, 2018 at 08:28In stm32l053 systick is not working with internal oscillator. I defined variable in systick interrupt and i configured HSI clock, but software broke on my delay function in main. I read all documentations about stm32...

USB HS for Mass storage and CDC combination

Posted on April 18, 2018 at 05:34I'm going to use USB HS in chip STM32F779 for both Mass storage and CDC interface . Can I know is it impossible ? And how to approach this solution ?

Hau Lam by Associate II
  • 835 Views
  • 0 replies
  • 0 kudos

Virtual Device for STM32

Posted on April 11, 2018 at 15:14Hi All,We at https://www.jumper.io are building virtual devices to help embedded software developers ship better code faster. Our mission is to make it fast and easy to automate testing and adopt agile and continuous...

STM32F0 ADC Scan Int Issue

Posted on April 18, 2018 at 03:16Hi, I am trying to set up an STM32f030 to do ADC conversions on 4 channels using interrupts and no DMA. The first ADC input gets good values but the second ADC inf put is wonky.I used CubeMX to generate the code. I a...

Looking for simple CAN receive example for STM32F042

Posted on April 17, 2018 at 22:52I am looking for a simple CAN Receive example for the STM32F042.  The example I usually see cited (STM32072B_EVAL\Examples\CAN\CAN_Networking) is really all about sending a message when a button is pressed.I'm using ...

STM32 real time FIR filter from ADC samples

Posted on March 10, 2018 at 21:40Hello,I have a Nucleo-L476RG board and I'm trying to make a lowpass filter with the FIR function (using cmsis libraries) to filter the samples I get from the ADC in realtime. Then I'd like to get the processed signal...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.