2019-04-03 7:20 AM
I am using an STM32F205RGY6 and looking at possible fault conditions in my circuit. With the MCU powered down, is there a safe maximum negative current I could apply to PC5 ? Under fault conditions I could see -4.1mA relative to Vss (-3.3v and 796 Ohms).
2019-04-03 7:56 AM
Look in the data sheet, Tabel 11 and 12. -5 mA is possible, but observe remark 2 :
2. Negative injection disturbs the analog performance of the device. See note in Section 6.3.20: 12-bit ADC
characteristics.
2019-04-03 10:45 AM
Thanks, I was hoping that's what the table meant. I was worried that I might be exceeding the minimum input voltage spec., Vss-0.3 . And since I' was looking at a powered-down situation performance is not an issue.
Appreciate the help.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.