2023-01-08 3:40 AM
This is the first time I have used an STM32F4 board.
In the Discovery kit with STM32F407VG MCU I see "one digital microphone", but I don't understand if it's already integrated in the board or I have to buy it separately.
If it is included, can you tell me in which manual I can find its specifications?
User manual? Reference manual? I'm searching but with no results.
Thanks!
2023-01-08 4:06 AM
It is a MP45DT02 on the board (U9), not in the chip. See UM1472 user manual and schematics mb997-f407vgt6-b02_schematic.pdf (revision code may vary).
hth
KnarfB
2023-01-08 6:06 AM
Thanks!
I have a couple of questions:
1) In the UM1472 (rev.7) user manual there's written that "Revision E-01" replaces the MP45DT02-M microphone (U9) with the IMP34DT05TR.
It is not clear to me which of these two microphones I have on board on my board.
2) I checked all the official documentation of the STM32F407-DISC1 but only found informations about the microphone in the application note AN3997 'Audio-playback-and-recording' which provides an example and the related library explained in AN3998 'PDM-audio-software-decoding'.
I will study these files but ask if you know of any other files/tutorials that explain the mic implementation step by step.
2023-01-08 6:58 AM
1) the revision letter is in the top right corner of the board M997..
2) no, but I haven't done a deep search.
hth
KnarfB
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.