2018-10-18 9:22 PM
I am trying to use RTC to wake up my stop mode every 30 second.
I have two questions:
so every time when RTC wakes up, I use below code to
HAL_RTC_DeInit(&hrtc);:
MX_RTC_Init( true );
to reinit RTC, and I don't use the interrupt handler.
It appears working fine, but I am not sure any risk of this.
My second question is I am a little confused about the RTC configuration.
I want a 15 s interval alarm for stop mode and a 24 hour alarm for standby mode.
So my code like below, but I know it is wrong, but not sure what went wrong.
I use LSI 40K RTC clock.
void MX_RTC_Init(bool stopMode)
{
RTC_TimeTypeDef sTime;
RTC_DateTypeDef sDate;
RTC_AlarmTypeDef sAlarm;
/**Initialize RTC Only
*/
hrtc.Instance = RTC;
hrtc.Init.HourFormat = RTC_HOURFORMAT_24;
hrtc.Init.AsynchPrediv = 127;
hrtc.Init.SynchPrediv = 319;
hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
if (HAL_RTC_Init(&hrtc) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/**Initialize RTC and set the Time and Date
*/
sTime.Hours = 0x0;
sTime.Minutes = 0x0;
sTime.Seconds = 0x0;
sTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
sTime.StoreOperation = RTC_STOREOPERATION_RESET;
if (HAL_RTC_SetTime(&hrtc, &sTime, RTC_FORMAT_BCD) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
sDate.WeekDay = RTC_WEEKDAY_MONDAY;
sDate.Month = RTC_MONTH_JANUARY;
sDate.Date = 0x1;
sDate.Year = 0x0;
if (HAL_RTC_SetDate(&hrtc, &sDate, RTC_FORMAT_BCD) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
if(HAL_RTCEx_BKUPRead(&hrtc, RTC_BKP_DR0) != 0x32F2){
HAL_RTCEx_BKUPWrite(&hrtc,RTC_BKP_DR0,0x32F2);
}
/**Enable the Alarm A
*/
sAlarm.AlarmTime.Minutes = 0x0;
if(stopMode)
{
sAlarm.AlarmTime.Hours = 0x0;
sAlarm.AlarmTime.Seconds = 15;
sAlarm.AlarmMask =RTC_ALARMMASK_SECONDS;
}
else
{
sAlarm.AlarmTime.Hours = 23;
sAlarm.AlarmTime.Seconds = 0;
sAlarm.AlarmMask = RTC_ALARMMASK_HOURS;
}
sAlarm.AlarmTime.SubSeconds = 0x0;
sAlarm.AlarmTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
sAlarm.AlarmTime.StoreOperation = RTC_STOREOPERATION_RESET;
sAlarm.AlarmSubSecondMask = RTC_ALARMSUBSECONDMASK_ALL;
sAlarm.AlarmDateWeekDaySel = RTC_ALARMDATEWEEKDAYSEL_DATE;
sAlarm.AlarmDateWeekDay = 0x1;
sAlarm.Alarm = RTC_ALARM_A;
if (HAL_RTC_SetAlarm_IT(&hrtc, &sAlarm, RTC_FORMAT_BCD) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.