2025-05-30 5:46 AM
Hello,
My agenda is to work with ADC1 with STOP2 mode.
Using LPTIMER1 to wakeup system, from STOP2 mode and once wakeup then reinit adc, calibrate and start adc interrupt. but still I can see adc interrupt not called.
void handleConversion()
{
ReInit_ADC1();
HAL_ADCEx_Calibration_Start(&hadc_);
HAL_StatusTypeDef status = HAL_ADC_Start_IT(&hadc1);
if (status != HAL_OK) {
HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_5);
}
// LED toggle if we put out of IF statement, so interrupt is register successfully.
} void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef *hadc)
{
__IO uint16_t adcRawValue = HAL_ADC_GetValue(hadc);
uint16_t adcVoltage_mVolt = __LL_ADC_CALC_DATA_TO_VOLTAGE(VDDA_APPLI, adcRawValue, LL_ADC_RESOLUTION_12B);
InternalBatteryDriver::setVoltageCallback(adcVoltage_mVolt);
// HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_5);
scheduler_push_event(EVENT_ADC_CONVERSION_COMPLETE);
}
//Here as final result, trying to glow LED which is not blinkingand here is the ADC_Init code for reference
static void MX_ADC1_Init(void)
{
ADC_ChannelConfTypeDef sConfig = {0};
hadc1.Instance = ADC1;
hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV4;
hadc1.Init.Resolution = ADC_RESOLUTION_12B;
hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc1.Init.ScanConvMode = ADC_SCAN_DISABLE;
hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
hadc1.Init.LowPowerAutoWait = ENABLE;
hadc1.Init.LowPowerAutoPowerOff = ENABLE;
hadc1.Init.ContinuousConvMode = DISABLE;
hadc1.Init.NbrOfConversion = 1;
hadc1.Init.DiscontinuousConvMode = DISABLE;
hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc1.Init.DMAContinuousRequests = DISABLE;
hadc1.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;
hadc1.Init.SamplingTimeCommon1 = ADC_SAMPLETIME_79CYCLES_5;
hadc1.Init.SamplingTimeCommon2 = ADC_SAMPLETIME_79CYCLES_5;
hadc1.Init.OversamplingMode = DISABLE;
hadc1.Init.TriggerFrequencyMode = ADC_TRIGGER_FREQ_HIGH;
if (HAL_ADC_Init(&hadc1) != HAL_OK)
{
Error_Handler();
}
sConfig.Channel = ADC_CHANNEL_4;
sConfig.Rank = ADC_REGULAR_RANK_1;
sConfig.SamplingTime = ADC_SAMPLINGTIME_COMMON_1;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
}Help me if I'm missing anything here.
FYI, this works when we try to disable stop2 mode.
Here is the wakeup details,
void enterLowPowerMode()
{
HAL_UARTEx_EnableStopMode(&hlpuart1);
HAL_SuspendTick();
HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI);
HAL_ResumeTick();
Reset_SystemClock();
}void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE2);
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_LSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.LSIState = RCC_LSI_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
{
Error_Handler();
}
}Thanks,
Nitin
Solved! Go to Solution.
2025-06-03 5:34 AM
Hello,
It is working now; I have missed the ADC interrupt handler to set.
Thanks,
Nitin
2025-05-30 6:20 AM - edited 2025-05-30 6:23 AM
Was the ADC working before going to sleep?
EDIT: Sorry - I missed where you said it did work.
@npatil15 wrote:Here is the wakeup details,
void enterLowPowerMode()
{
HAL_UARTEx_EnableStopMode(&hlpuart1);
HAL_SuspendTick();
HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI);
HAL_ResumeTick();
Reset_SystemClock();
}
You haven't shown the code of Reset_SystemClock()
2025-06-01 10:04 PM - edited 2025-06-01 10:07 PM
actually Reset_SystemClock() is just the wrapper for SystemClock_Config() function.
void Reset_SystemClock(void)
{
SystemClock_Config()
}And ReInit_ADC1() is also a wrapper function for MX_ADC1_Init()
void ReInit_ADC1(void)
{
MX_ADC1_Init();
}Thanks,
Nitin
2025-06-02 2:15 AM
Seems like unnecessary obfuscation - why not just call the functions direct?
2025-06-02 10:52 PM
This I have done for purpose, as have multiple CPP and C file.
2025-06-03 5:34 AM
Hello,
It is working now; I have missed the ADC interrupt handler to set.
Thanks,
Nitin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.