2020-12-03 5:12 AM
Hello @Community member @All ALL @Alexandre Allien
Currently, I am using STM32F412CGU6 Microcontroller along with External FLASH(W25Q32JVSSIQ).
The External Flash(W25Q32JVSSIQ) supports QSPI interface for fast reading of data.
I would like to interface STM32F412CGU6 Microcontroller with external flash (W25Q32JVSSIQ) in QSPI interface.
The STM32F412CGU6 Microcontroller does not have physical pin IO2(QUADSPI_BK2_IO2) & IO3.( QUADSPI_BK2_IO3).
Is there any alternate solution that can help me to use the QSPI interface ?
Is it possible that I can use the GPIO line PA15 and PA8 as IO2 and IO3 respectively?
Should I modified the "HAL_QSPI_MspInit" API with following change?
/* QSPI D2 GPIO pin configuration */
GPIO_InitStruct.Pin = GPIO_PIN_15;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* QSPI D3 GPIO pin configuration */
GPIO_InitStruct.Pin = GPIO_PIN_8;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
Please guide me for same.
Regards,
Nikunj Patel
2020-12-03 10:02 AM
You can't randomly assign pins.
48UFQFPN Right? Picked the wrong part to do QSPI, AF mappings totally unhelpful
@STOne-32 Really need to bang some heads about coming up with workable AF mappings on these lower pin count devices.
2020-12-07 1:42 AM
Hello @Community member @All ALL @Alexandre Allien
yes, I am using "UFQFPN48" package and I am totally agree with your answer.
please, let me know that "Can I use "Dual SPI" instead of "Standard SPI" for STM32F412CGU6 ".
If Dual SPI possible.
If possible, Please, Provide me any link or sample example for Dual SPI configuration.
Regards,
Nikunj Patel
2020-12-07 5:27 AM
Dual in that context would be two FLASH IC's
With NCS,CLK,IO0, and IO1 the 2-bit "dual" commands/mode might function. ie 2 LINE modes for CMD, ADDR, DATA
You'd probably want to try wiring up a test fixture and double check before committing to a PCB
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.