STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

flash access through ART or not

Hello,I was looking to the docs about flash/ART accelerator, and it was saying access through ART is only if done through ITCM not through AXI, and ITCM access is through 0020 0000. The (default project) linker description (of STM32CubeIDE) only has ...

mete by Senior II
  • 1238 Views
  • 2 replies
  • 0 kudos

strange behavior when flashing in RAM

I write a program, send 0x55 via UART, and set the system timer for 1000 calls per second.the program is recorded to FLASH and works as expected.then I change the address for the firmware in the linker, instead of the flash drive I write to RAM.I cha...

Resolved! STM32G474 DMA Transfer Error and DAC underrun

Hi,I am trying to write a waveform table to the DAC peripheral using DMA and the TIM6 peripheral.TIM6 does appear to work as expected.I can also see the DMA getting triggered by means of TIM6_TRGO.But the DMA Transfer results in a Transfer Error, res...

Why is this happening to the I2S bus?

Hi guys, Finally started injected known data into the I2S bus and I am seeing indifferences on the line and was wondering if you guys can explain this to me if this is normal or not.Using the STM32H753ZIFigure 1:Sending: 0xFF FF (16 bits) DATLEN = 16...

0693W000006Em06QAC.png 0693W000006Em0kQAC.png 0693W000006Em0uQAC.png
CLeo.1 by Senior II
  • 1862 Views
  • 4 replies
  • 0 kudos

Resolved! STM32L412KB ADC Oversampling - Question to right bitshift

Hello,i am using ADC with DMA. In my initialization code i did the ADC calibration procedure like that: HAL_ADCEx_Calibration_Start(&hadc1, ADC_SINGLE_ENDED); // ADC calibration VrefintCalValue = (*VREFINT_CAL_ADDR); // read out the calibratio...

ledi001 by Senior
  • 2589 Views
  • 1 replies
  • 1 kudos

File read in STM32

Hi, We are from Nagra IOT team currently working on IOT products based on STM boards.We are using SMT32L4 (B-L475E-IOT01A1).Our current requirement is putting a file in ST board - in flash preferably and read it using simple file I/O operations like ...

Asama.11 by Associate
  • 1270 Views
  • 0 replies
  • 0 kudos

looking for Model Based Development Tool

Hello ​I am looking for free MBD tool for programming. ​I think Algobuilder is good. but cpu is limited and dedicated only for mems sensors. ​I found MBD tool xcos based on Scilab. and module for cubemx, codegenator.https://atoms.scilab.org/toolbo...

kdok .1 by Associate II
  • 1276 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.