2024-03-14 1:59 AM
Hello
I am trying to do spi_dma communication using the HAL_SPI_TransmitReceive_DMA function.
When I use HAL_SPI_TransmitReceive_DMA in a situation where I use the same dma stream, same amount of data to send and receive, but different addresses to send and receive,
Is there any part of the code in the HAL_SPI_TransmitReceive_DMA function that only needs to be set once?
If so, is it possible to separate the actual behavior code of the HAL_SPI_TransmitReceive_DMA function and the code that only needs to be set once from HAL_SPI_TransmitReceive_DMA to execute HAL_SPI_TransmitReceive_DMA?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.