2010-06-14 10:38 AM
IPSR information for STM32F107
2011-05-17 4:54 AM
+2e .word TIM4_IRQHandler
2011-05-17 4:54 AM
From what documentation did you find out that 0x2e is the TIM4 interrupt?
2011-05-17 4:54 AM
I did the math. See also http://plex-svn.googlecode.com/svn-history/r405/trunk/h103/3rd_party/stm/CMSIS/Core/CM3/startup/arm/startup_stm32f10x_hd.s
+g_pfnVectors: +00 .word Initial_spTop +01 .word Reset_Handler +02 .word NMI_Handler +03 .word HardFault_Handler +04 .word MemManage_Handler +05 .word BusFault_Handler +06 .word UsageFault_Handler +07 .word 0 +08 .word 0 +09 .word 0 +0a .word 0 +0b .word SVC_Handler +0c .word DebugMon_Handler +0d .word 0 +0e .word PendSV_Handler +0f .word SysTick_Handler +10 .word WWDG_IRQHandler +11 .word PVD_IRQHandler +12 .word TAMPER_IRQHandler +13 .word RTC_IRQHandler +14 .word FLASH_IRQHandler +15 .word RCC_IRQHandler +16 .word EXTI0_IRQHandler +17 .word EXTI1_IRQHandler +18 .word EXTI2_IRQHandler +19 .word EXTI3_IRQHandler +1a .word EXTI4_IRQHandler +1b .word DMA1_Channel1_IRQHandler +1c .word DMA1_Channel2_IRQHandler +1d .word DMA1_Channel3_IRQHandler +1e .word DMA1_Channel4_IRQHandler +1f .word DMA1_Channel5_IRQHandler +20 .word DMA1_Channel6_IRQHandler +21 .word DMA1_Channel7_IRQHandler +22 .word ADC1_2_IRQHandler +23 .word USB_HP_CAN1_TX_IRQHandler +24 .word USB_LP_CAN1_RX0_IRQHandler +25 .word CAN1_RX1_IRQHandler +26 .word CAN1_SCE_IRQHandler +27 .word EXTI9_5_IRQHandler +28 .word TIM1_BRK_IRQHandler +29 .word TIM1_UP_IRQHandler +2a .word TIM1_TRG_COM_IRQHandler +2b .word TIM1_CC_IRQHandler +2c .word TIM2_IRQHandler +2d .word TIM3_IRQHandler +2e .word TIM4_IRQHandler +2f .word I2C1_EV_IRQHandler +30 .word I2C1_ER_IRQHandler +31 .word I2C2_EV_IRQHandler +32 .word I2C2_ER_IRQHandler +33 .word SPI1_IRQHandler +34 .word SPI2_IRQHandler +35 .word USART1_IRQHandler +36 .word USART2_IRQHandler +37 .word USART3_IRQHandler +38 .word EXTI15_10_IRQHandler +39 .word RTCAlarm_IRQHandler +3a .word USBWakeUp_IRQHandler +3b .word TIM8_BRK_IRQHandler +3c .word TIM8_UP_IRQHandler +3d .word TIM8_TRG_COM_IRQHandler +3e .word TIM8_CC_IRQHandler +3f .word ADC3_IRQHandler +40 .word FSMC_IRQHandler +41 .word SDIO_IRQHandler +42 .word TIM5_IRQHandler +43 .word SPI3_IRQHandler +44 .word UART4_IRQHandler +45 .word UART5_IRQHandler +46 .word TIM6_IRQHandler +47 .word TIM7_IRQHandler +48 .word DMA2_Channel1_IRQHandler +49 .word DMA2_Channel2_IRQHandler +4a .word DMA2_Channel3_IRQHandler +4b .word DMA2_Channel4_5_IRQHandler +4c .word 0 +4d .word 0 +4e .word 0 +4f .word 0 +50 .word 0 +51 .word 0 +52 .word 0 +53 .word 0We’re moving the ST Community to a new platform to give you a better and more reliable community experience.