2009-10-05 7:18 AM
internal pull up on 5 volt pin
2011-05-17 4:25 AM
Hi all,
Is it OK to enable internal pull up on port pin that could be exposed to 5 volts? The pin is a five volt tolerant pin. I presume the internal pull resistor is connected to VDD (3v3 in my case) therefore there would be a small current flowing from the port pin (5V) through the internal pull up to 3v3. It works but I was just wondering if it might damage the processor in time. Regards Trevor2011-05-17 4:25 AM
I'd stick to maximum ratings in the datasheet: max. current in/out, max. voltage. There is most probably no danger.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.