2026-01-05 5:20 PM
Hi experts:
I'm working on STM32U575 evk, using ADC1 including two channels enabe interrupt, attached file is my test project, only one interrupt in the callback function, I don't know why, if I changed the end of conversion selection to end of sequence of conversion, no interrupt triggered, please help to check if anything missing in my project, thanks.
Bill
2026-01-12 1:09 AM
Hello @lbapplem
Your project "test_adc_evk" is correct.
Selection of end of conversion/sequence interruption is done in fie "adc.c":
- setting "hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;" will make ADC interruption trig at each end of conversion (EOC)
- setting "hadc1.Init.EOCSelection = ADC_EOC_SEQ_CONV;" will make ADC interruption trig at each end of sequence (EOS)
This configuration is done in function "HAL_ADC_Start_IT()":
/* Enable ADC end of conversion interrupt */
switch (hadc->Init.EOCSelection)
{
case ADC_EOC_SEQ_CONV:
__HAL_ADC_ENABLE_IT(hadc, ADC_IT_EOS);
break;
/* case ADC_EOC_SINGLE_CONV */
default:
__HAL_ADC_ENABLE_IT(hadc, ADC_IT_EOC);
break;
}
Since interruption is working for initial setting EOC, there is no reason to not work for EOS.
Debug suggestion :
1. Watch ADC status register (SR) flags: when the 2 conversions of the sequence are done, flag EOS should be == 1
Can also be done with "LL_ADC_IsActiveFlag_EOS()".
2. In your current project, after start IT (only for debug), add:
LL_ADC_DisableIT_EOC();
LL_ADC_EnableIT_EOS();
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.