2017-01-24 1:25 PM
I asked a question earlier on how to generate n-Pulses from STM32 to drive a servo like interface ->
https://community.st.com/0D50X00009XkdsSSAR
, and it worked. This feature is available only on TIM1/8. Is there a novel way of interfacing 5 motors to one F7?I am trying to interface 5 Teknic Clearpath SDSK motors to STM32F7 Nucleo Dev Board. They are Brushless DC motors with a stepper like interface. The motor moves a set distance based on the number of pulses it receives. The speed is determined by the frequency of the pulses, like a stepper motor.
I can hook up the two motors to TIM1 and 8, and the rest with a feedback to counter,. DMA buffering won't work, as I rely on the pulses sent to determine the current position of the motor. I am just looking for a better solution here.
#stm32-pwm-timers #n-pulse2017-01-25 3:00 PM
That leaves us mostly with the two timers in master-slave arrangement, master gating the slave. Besides TIM1 and TIM8, which are good as they are alone, there are 2 pairs of timers in TIM2..TIM5 and 2 pairs in TIM9..TIM12 possible, that's 6 which is more than you require.
JW
2017-01-25 5:43 PM
This would be a great use of the motion control microcode package for the TPU on a MC68332 or PowerPC chip. But it would only be able to handle 16 or 32 channels of this stuff simultaneously.
Unfortunately the ST ARM chips don't do multi-channel motor control very nicely. You're going to have to add some extra hardware, whether processors or motor controllers.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.