2025-01-22 5:40 AM
Dear community,
my Nucleo H723ZG captures analog signals via channels (see attachment) :
The second one reads a 4-20mA pressure signal from a sensor with the help of an external shunt resistor. After a system reset/reboot, the voltage there is now frozen at 0.021mA which is weird and I start suspecting that this specific analog input port has some issue...Could it be, that the input impedance of analog input ports is configurable and might go to a different state after a reset or software reboot?
Thanks in advance
Kind regards
2025-01-22 6:38 AM
Q: .Could it be, that the input impedance of analog input ports is configurable and might go to a different state after a reset or software reboot?
A: No. Analog input or ADC could be damaged, since your circuits very primitive and doesn't protect uCPU against overvoltage.
You may try to test input to adc using potentiometer.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.