STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Unable to detect target - STM32H503

Hi, I have STM32H503 mounted on my board and to trying flash the code via SWD line. However, the tool says target not detected. The supply lines show 3.3V and boot pin is grounded.  I am using pins- SWDIO, SWCLK, RESET and GND. 

Problem with UART in secure and unprivileged mode U5

Hello,I'm currently tring to do an app and I want to switch in unprivileged mode when I'm in secure and privileged mode. The switch is working but the uart is not working in unprivileged mode. It works in privileged mode. When I debug my code go in t...

ECoud.1 by Associate III
  • 1525 Views
  • 2 replies
  • 0 kudos

Issues with library of G431

Hi, after spending already the half day, i finally found one problem of multiple:https://github.com/STMicroelectronics/cmsis-device-g4/blob/master/Include/stm32g431xx.hLine 1029 continues with wrong offset. Should be 18. Following are wrong too.After...

Tobe by Senior III
  • 2555 Views
  • 7 replies
  • 6 kudos

Input resistance of analog input, reset (?)

Dear community, my Nucleo H723ZG captures analog signals via channels (see attachment) :ADC12_INP15,ADC12_INP10 andADC12_INP10 The second one reads a 4-20mA pressure signal from a sensor with the help of an external shunt resistor. After a system res...

LysAn by Associate III
  • 1424 Views
  • 1 replies
  • 1 kudos

BootLoader timeout

Posted on January 12, 2015 at 09:17HiI am using STM32L151 bootloader.I wanted to run the bootloader at program start, and if no usb if attached for a certain timego back to regular application.Is it possible to configure a timeout for the bootloader...

yarona by Associate II
  • 2439 Views
  • 4 replies
  • 3 kudos

stm32h7 dual core debugging

Hi all. I am using STM32H747BIT6 with cm4 & cm7 cores but I am struggling with debugging my application. I started a new STM32 project using the CubeIDE wizard and gave the ioc file to generate simple code. Then I built the two projects (m4 & m7). Af...

yonatan by Associate III
  • 2049 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.