2018-12-31 10:07 PM
I have 7 adc channel must be measured. 4 channels are continuously measured by dma and adc 1, 3 of them are very important measured in special moment. I want to mesured this channels by injected channel adc2. my code for this as follow, but I can not mesured injected channels in adc2 and regular channels in adc1.
configuration of GPIO as follow:
void ADC1_GPIO_Config(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOC, ENABLE);
// GPIO Init for regular channels
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0|GPIO_Pin_1;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AIN;
GPIO_Init(GPIOA, &GPIO_InitStructure);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_3|GPIO_Pin_4;
GPIO_Init(GPIOC, &GPIO_InitStructure);
// GPIO Init for injected channels
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0|GPIO_Pin_1|GPIO_Pin_2;
GPIO_Init(GPIOC, &GPIO_InitStructure);
}and configuration of DMA is:
void DMA1_Mode_Config(void)
{
DMA_InitTypeDef DMA_InitStructure;
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE);
/* DMA channel1 configuration */
DMA_DeInit(DMA1_Channel1);
DMA_InitStructure.DMA_M2M = DMA_M2M_Disable;
DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;
DMA_InitStructure.DMA_Priority = DMA_Priority_High;
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC;
DMA_InitStructure.DMA_BufferSize = 4;
DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&ADC1->DR;;
DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t) &ADC_ConvertedValue;
DMA_Init(DMA1_Channel1, &DMA_InitStructure);
DMA_Cmd(DMA1_Channel1, ENABLE);
}configuration of ADC1 is:
void ADC1_Mode_Config(void)
{
ADC_InitTypeDef ADC_InitStructure;
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);
ADC_InitStructure.ADC_Mode = ADC_Mode_RegSimult;
ADC_InitStructure.ADC_ScanConvMode = ENABLE;
ADC_InitStructure.ADC_ContinuousConvMode = ENABLE;
ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_None;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_NbrOfChannel = 7;
ADC_Init(ADC1, &ADC_InitStructure);
ADC_RegularChannelConfig(ADC1, ADC_Channel_0, 1, ADC_SampleTime_1Cycles5);
ADC_RegularChannelConfig(ADC1, ADC_Channel_1, 2, ADC_SampleTime_1Cycles5);
ADC_RegularChannelConfig(ADC1, ADC_Channel_13,3, ADC_SampleTime_1Cycles5);
ADC_RegularChannelConfig(ADC1,ADC_Channel_14, 4, ADC_SampleTime_1Cycles5);
ADC_DMACmd(ADC1, ENABLE);
ADC_Cmd(ADC1, ENABLE);
ADC_ResetCalibration(ADC1);
while(ADC_GetResetCalibrationStatus(ADC1));
ADC_StartCalibration(ADC1);
while(ADC_GetCalibrationStatus(ADC1));
ADC_SoftwareStartConvCmd(ADC1, ENABLE);
}
void ADC1_Init(void)
{
ADC1_GPIO_Config();
DMA1_Mode_Config();
ADC1_Mode_Config();
}and configuration of ADC2 is:
void ADC2_Init_MSS(void)
{
ADC_InitTypeDef ADC_InitStructure;
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC2, ENABLE);
/* ADC2 configuration */
ADC_InitStructure.ADC_Mode = ADC_Mode_InjecSimult;
ADC_InitStructure.ADC_ScanConvMode = ENABLE;
ADC_InitStructure.ADC_ContinuousConvMode = DISABLE;
ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_None;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_NbrOfChannel = 3;
ADC_Init(ADC2, &ADC_InitStructure);
ADC_InjectedChannelConfig(ADC2,ADC_Channel_10,1,ADC_SampleTime_1Cycles5);
ADC_InjectedChannelConfig(ADC2,ADC_Channel_11,2,ADC_SampleTime_1Cycles5);
ADC_InjectedChannelConfig(ADC2,ADC_Channel_12,3,ADC_SampleTime_1Cycles5);
ADC_InjectedSequencerLengthConfig(ADC2,3);
ADC_InjectedSequencerLengthConfig(ADC2,3);
ADC_ResetCalibration(ADC2);
while(ADC_GetResetCalibrationStatus(ADC2));
ADC_StartCalibration(ADC2);
while(ADC_GetCalibrationStatus(ADC2));
ADC_SoftwareStartConvCmd(ADC2, ENABLE);
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.