2017-07-20 4:50 PM
Hi All,
I'm using the advanced timer TIM1 on STM32303VC to drive a 2 phase shifted full bridges separated by a transformer (Dual Active Bridge topology). This required use of 4 PWMs. CH1 and CH1N drive the primary bridge. CH3 and CH3N drive the secondary bridge.
The question is I need to program independent dead times (for CH1-CH1N and CH3-CH3N). Is that possible? Because the LL APIs have only one dead time configuration value per Timer.
If it's not possible what is the workaround? This is a make or break situation for my converter.
Regards,
Vivek
#phase-shift #advanced-timers #timer-synchronizationSolved! Go to Solution.
2017-07-21 1:53 AM
The question is I need to program independent dead times (for CH1-CH1N and CH3-CH3N). Is that possible?
No.
If it's not possible what is the workaround?
Using two different timers?
JW
2017-07-21 1:53 AM
The question is I need to program independent dead times (for CH1-CH1N and CH3-CH3N). Is that possible?
No.
If it's not possible what is the workaround?
Using two different timers?
JW
2017-07-21 7:27 AM
Thanks JW.
Can I apply phase shift if I drive the bridges using two different timers? Also I need to apply this work around in my existing hardware. So that means I can configure Tim1_ch3-ch3n as input high impedance and short it with Tim8_ch1-ch1n. That should work right?
2017-07-24 6:04 PM
Vivek,
The STM32F334 has the HRTIM with an independent deadtime control for each channel.
Why your phase shift bridge need independent deadtime?
Ari.
2017-07-24 6:39 PM
2017-07-25 3:58 AM
Thanks for sharing your solution.
The reference manual mentions resynchronization delay but it never mentions what value will this resync. delay be.
Good question; I've never seen the inter-timer TRGO-TRGI delay properly specified - maybe in some of the appnotes?. TIMx_SMCR.MSM bit description vaguely hints about delaying the effect of TRGI ' to allow a perfect synchronization between the current timer and its slaves'; I've never tried that either.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.